CloseRangeDemoCylinderListItemBuilder Class¶
-
class
NXOpen.Features.VehicleDesign.
CloseRangeDemoCylinderListItemBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents the builder to create demo cylinder list item used for close range visibility.
To create a new instance of this class, use
NXOpen.Features.VehicleDesign.CloseRangeVisibilityBuilder.CreateDemoCylinderListItemBuilder()
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
PositionOnPath | Returns the percentage value of position on demo cylinder path to define the demo cylinder. |
ShowDemoCylinder | Returns or sets the indication if demo cylinder will be shown. |
ShowDemoCylinderRay | Returns or sets the indication if demo cylinder ray will be shown. |
Tag | Returns the Tag for this object. |
ValidateType | Returns or sets the validate checking types to define the close range visibility for the demo cylinders. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
CloseRangeDemoCylinderListItemBuilderValidateTypes Enumeration | This enum represents the simple or detailed checking options to validate demo cylinders visibility. |
Property Detail¶
PositionOnPath¶
-
CloseRangeDemoCylinderListItemBuilder.
PositionOnPath
¶ Returns the percentage value of position on demo cylinder path to define the demo cylinder.
-------------------------------------
Getter Method
Signature
PositionOnPath()
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
ShowDemoCylinder¶
-
CloseRangeDemoCylinderListItemBuilder.
ShowDemoCylinder
¶ Returns or sets the indication if demo cylinder will be shown.
-------------------------------------
Getter Method
Signature
ShowDemoCylinder()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShowDemoCylinder(showDemoCylinder)
Parameters: showDemoCylinder (bool) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
ShowDemoCylinderRay¶
-
CloseRangeDemoCylinderListItemBuilder.
ShowDemoCylinderRay
¶ Returns or sets the indication if demo cylinder ray will be shown.
-------------------------------------
Getter Method
Signature
ShowDemoCylinderRay()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShowDemoCylinderRay(showDemoCylinderRay)
Parameters: showDemoCylinderRay (bool) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
ValidateType¶
-
CloseRangeDemoCylinderListItemBuilder.
ValidateType
¶ Returns or sets the validate checking types to define the close range visibility for the demo cylinders.
-------------------------------------
Getter Method
Signature
ValidateType()
Returns: Return type: NXOpen.Features.VehicleDesign.CloseRangeDemoCylinderListItemBuilderValidateTypes
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ValidateType(validateType)
Parameters: validateType ( NXOpen.Features.VehicleDesign.CloseRangeDemoCylinderListItemBuilderValidateTypes
) –New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
Method Detail¶
Validate¶
-
CloseRangeDemoCylinderListItemBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.