CloseRangeDemoCylinderListItemBuilderValidateTypes Enumeration

NXOpen.Features.VehicleDesign.CloseRangeDemoCylinderListItemBuilder.ValidateTypes is an alias for NXOpen.Features.VehicleDesign.CloseRangeDemoCylinderListItemBuilderValidateTypes

class NXOpen.Features.VehicleDesign.CloseRangeDemoCylinderListItemBuilderValidateTypes

Bases: object

This enum represents the simple or detailed checking options to validate demo cylinders visibility.

Enum Members

Enum Member Enum Member Description
Simple
Simple type
Detailed
Detailed type
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.