UserDefinedFeatureCreateEvent Class

class NXOpen.Features.UserDefinedFeatureCreateEvent

Bases: NXOpen.TaggedObject

JA interface for the UserDefinedFeatureCreateEvent object

This calls cannot be created

New in version NX8.0.0.

Properties

Property Description
ApplicationData Returns the application data
ClassName Returns the class name
CopiedFeature Returns the feature in the destination part
Definition Returns the user defined feature definition
OriginalFeature Returns the original feature being copied
Tag Returns the Tag for this object.

Methods

Method Description
GetComponentFeatures The component features that have been created so far @return
GetExpressionData The expressions of the instantiation feature @return
GetReferenceData The references of the instantiation feature @return

Property Detail

ApplicationData

UserDefinedFeatureCreateEvent.ApplicationData

Returns the application data

-------------------------------------

Getter Method

Signature ApplicationData()

Returns:the application data
Return type:NXOpen.Features.UserDefinedFeatureApplicationData

New in version NX8.0.0.

License requirements: None.

ClassName

UserDefinedFeatureCreateEvent.ClassName

Returns the class name

-------------------------------------

Getter Method

Signature ClassName()

Returns:
Return type:str

New in version NX8.0.0.

License requirements: None.

CopiedFeature

UserDefinedFeatureCreateEvent.CopiedFeature

Returns the feature in the destination part

-------------------------------------

Getter Method

Signature CopiedFeature()

Returns:The feature being copied
Return type:NXOpen.Features.Feature

New in version NX8.0.0.

License requirements: None.

Definition

UserDefinedFeatureCreateEvent.Definition

Returns the user defined feature definition

-------------------------------------

Getter Method

Signature Definition()

Returns:The UDF definition that is being created
Return type:NXOpen.Features.Feature

New in version NX8.0.0.

License requirements: None.

OriginalFeature

UserDefinedFeatureCreateEvent.OriginalFeature

Returns the original feature being copied

-------------------------------------

Getter Method

Signature OriginalFeature()

Returns:The feature being copied
Return type:NXOpen.Features.Feature

New in version NX8.0.0.

License requirements: None.

Method Detail

GetComponentFeatures

UserDefinedFeatureCreateEvent.GetComponentFeatures

The component features that have been created so far

Signature GetComponentFeatures()

Returns:
Return type:list of NXOpen.Features.Feature

New in version NX8.0.0.

License requirements: None.

GetExpressionData

UserDefinedFeatureCreateEvent.GetExpressionData

The expressions of the instantiation feature

Signature GetExpressionData()

Returns:
Return type:list of NXOpen.Features.UserDefinedFeatureExpressionData

New in version NX8.0.0.

License requirements: None.

GetReferenceData

UserDefinedFeatureCreateEvent.GetReferenceData

The references of the instantiation feature

Signature GetReferenceData()

Returns:
Return type:list of NXOpen.Features.UserDefinedFeatureReferenceData

New in version NX8.0.0.

License requirements: None.