UserDefinedFeatureReferenceData Class

class NXOpen.Features.UserDefinedFeatureReferenceData

Bases: NXOpen.TaggedObject

JA interface for UserDefinedFeatureReference object.

Objects of this class contain an external reference of the user defined feature and the corresponding prompt. This cannot be created

New in version NX8.0.0.

Properties

Property Description
Prompt Returns the prompt for this reference
Reference Returns the reference of a user defined feature
Tag Returns the Tag for this object.

Methods

Property Detail

Prompt

UserDefinedFeatureReferenceData.Prompt

Returns the prompt for this reference

-------------------------------------

Getter Method

Signature Prompt()

Returns:the prompt for this reference
Return type:str

New in version NX8.0.0.

License requirements: None.

Reference

UserDefinedFeatureReferenceData.Reference

Returns the reference of a user defined feature

-------------------------------------

Getter Method

Signature Reference()

Returns:the reference of a user defined feature
Return type:NXOpen.TaggedObject

New in version NX8.0.0.

License requirements: None.