TrackingData Class¶
-
class
NXOpen.Features.
TrackingData
¶ Bases:
NXOpen.TransientObject
JA interface for Tracking Data
An instance of this class can be obtained from
NXOpen.Features.CustomFeatureCreateFeatureGeometryEvent.CreateTrackingDataForParasolidEntity()
orNXOpen.Features.CustomFeatureCreateFeatureGeometryEvent.CreateTrackingDataForNXObject()
orNXOpen.Features.CustomFeatureModifyFeatureGeometryEvent.CreateTrackingDataForNXObject()
New in version NX11.0.0.
Methods¶
Method | Description |
---|---|
AddIntSourceEntity | Adds the source entity of integer type for tracked entity |
AddTagIntPairSourceEntity | Adds the source entity of NXOpen::Object - integer pair type for tracked entity |
AddTagSourceEntities | Adds the source entities of NXOpen::Object’s type for tracked entity |
Dispose | Frees the memory associated with this object. |
SetIntApplicationKey | Sets the optional application key of integer type for tracked entity |
SetNXOpenObjectApplicationKey | Sets the optional application key of NXOpen::Object type for tracked entity |
Method Detail¶
AddIntSourceEntity¶
-
TrackingData.
AddIntSourceEntity
¶ Adds the source entity of integer type for tracked entity
Signature
AddIntSourceEntity(sourceEntity)
Parameters: sourceEntity (int) – New in version NX11.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
AddTagIntPairSourceEntity¶
-
TrackingData.
AddTagIntPairSourceEntity
¶ Adds the source entity of NXOpen::Object - integer pair type for tracked entity
Signature
AddTagIntPairSourceEntity(tagSourceEntity, intSourceEntity)
Parameters: - tagSourceEntity (
NXOpen.NXObject
) – - intSourceEntity (int) –
New in version NX11.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
- tagSourceEntity (
AddTagSourceEntities¶
-
TrackingData.
AddTagSourceEntities
¶ Adds the source entities of NXOpen::Object’s type for tracked entity
Signature
AddTagSourceEntities(sourceEntities)
Parameters: sourceEntities (list of NXOpen.NXObject
) –New in version NX11.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Dispose¶
-
TrackingData.
Dispose
¶ Frees the memory associated with this object.
After invocation of this method, the object is no longer valid.
Signature
Dispose()
New in version NX11.0.0.
License requirements: None.
SetIntApplicationKey¶
-
TrackingData.
SetIntApplicationKey
¶ Sets the optional application key of integer type for tracked entity
Signature
SetIntApplicationKey(applicationKey)
Parameters: applicationKey (int) – New in version NX11.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SetNXOpenObjectApplicationKey¶
-
TrackingData.
SetNXOpenObjectApplicationKey
¶ Sets the optional application key of NXOpen::Object type for tracked entity
Signature
SetNXOpenObjectApplicationKey(applicationKey)
Parameters: applicationKey ( NXOpen.NXObject
) –New in version NX11.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)