CustomFeatureModifyFeatureGeometryEvent Class¶
-
class
NXOpen.Features.
CustomFeatureModifyFeatureGeometryEvent
¶ Bases:
NXOpen.Features.CustomFeatureEvent
JA interface for the CustomFeatureModifyFeatureGeometryEvent object
This calls cannot be created
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
ErrorCode | Returns or sets the error occured during the event |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
AppendOutputTrackingData | Add the tracking data for feature |
CreateTrackingDataForNXObject | Create the tracking data of the given NX object @return |
GetConstructionFeatures | The custom feature get construction features @return Output array of NXOpen Features |
GetCreatedBodies | A method to get parasolid bodies created custom feature in create geometry callback @return The Array of output Bodies |
GetCustomFeature | Get the custom feature of the event @return The owning Custom Feature of feature that caused the event to fire |
GetNXObject | Get the Parasolid tag of Solid body @return |
GetOutputFeatures | The output features created in post update event @return Output array of NXOpen Features |
GetParasolidId | Get the Parasolid tag of Solid body @return |
Getbodies | A method to get parasolid bodies of custom feature @return The Array of output Bodies |
Method Detail¶
AppendOutputTrackingData¶
-
CustomFeatureModifyFeatureGeometryEvent.
AppendOutputTrackingData
¶ Add the tracking data for feature
Signature
AppendOutputTrackingData(trackingData)
Parameters: trackingData (list of NXOpen.Features.TrackingData
) –New in version NX11.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
CreateTrackingDataForNXObject¶
-
CustomFeatureModifyFeatureGeometryEvent.
CreateTrackingDataForNXObject
¶ Create the tracking data of the given NX object
Signature
CreateTrackingDataForNXObject(nxObject)
Parameters: nxObject ( NXOpen.TaggedObject
) – The NX object for which create traking dataReturns: Return type: NXOpen.Features.TrackingData
New in version NX11.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
GetCreatedBodies¶
-
CustomFeatureModifyFeatureGeometryEvent.
GetCreatedBodies
¶ A method to get parasolid bodies created custom feature in create geometry callback
Signature
GetCreatedBodies()
Returns: The Array of output Bodies Return type: list of int New in version NX11.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)