SymmetricBuilder Class¶
-
class
NXOpen.Features.
SymmetricBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.Symmetric
builderTo create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateSymmetricBuilder()
Default values.
Property Value MoveAlongFace.CoaxialEnabled True MoveAlongFace.CoplanarAxesEnabled 0 MoveAlongFace.CoplanarEnabled True MoveAlongFace.EqualDiameterEnabled 0 MoveAlongFace.OffsetEnabled 0 MoveAlongFace.ParallelEnabled 0 MoveAlongFace.PerpendicularEnabled 0 MoveAlongFace.SymmetricEnabled 0 MoveAlongFace.TangentEnabled 0 MoveAlongFace.ThicknessChainEnabled 0 MoveAlongFace.UseFaceBrowse 1 SymmetryPlaneOption Existing New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
ExistingSymmetryPlane | Returns the existing symmetry plane. |
MotionFace | Returns the motion face. |
MoveAlongFace | Returns the move along face. |
NewSymmetryPlane | Returns or sets the new symmetry plane. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
StationaryFace | Returns the stationary face. |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
SymmetryPlaneOption | Returns or sets the symmetry plane option. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
SymmetricBuilderPlaneOptions Enumeration | Represents the plane options. |
Property Detail¶
ExistingSymmetryPlane¶
-
SymmetricBuilder.
ExistingSymmetryPlane
¶ Returns the existing symmetry plane.
The
NXOpen.SelectFace
object is employed to select existing planar face or datum plane as the symmetry plane if plane option is set toNXOpen.Features.SymmetricBuilderPlaneOptions.Existing
.-------------------------------------
Getter Method
Signature
ExistingSymmetryPlane()
Returns: Return type: NXOpen.SelectISurface
New in version NX6.0.0.
License requirements: None.
MotionFace¶
-
SymmetricBuilder.
MotionFace
¶ Returns the motion face.
The constraint is applied between the motion face and a stationary face. The motion face is transformed when the constraint is applied.
-------------------------------------
Getter Method
Signature
MotionFace()
Returns: Return type: NXOpen.SelectFace
New in version NX6.0.0.
License requirements: None.
MoveAlongFace¶
-
SymmetricBuilder.
MoveAlongFace
¶ Returns the move along face.
The
NXOpen.Features.FaceRecognitionBuilder
object is employed to collect tag-along faces. When the motion face is selected it is used as a seed for recognition of tag-along faces.-------------------------------------
Getter Method
Signature
MoveAlongFace()
Returns: Return type: NXOpen.Features.FaceRecognitionBuilder
New in version NX6.0.0.
License requirements: None.
NewSymmetryPlane¶
-
SymmetricBuilder.
NewSymmetryPlane
¶ Returns or sets the new symmetry plane.
The
NXOpen.Plane
object is employed to define the symmetry plane if plane option is set toNXOpen.Features.SymmetricBuilderPlaneOptions.New
.-------------------------------------
Getter Method
Signature
NewSymmetryPlane()
Returns: Return type: NXOpen.Plane
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NewSymmetryPlane(newSymmetryPlane)
Parameters: newSymmetryPlane ( NXOpen.Plane
) –New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
StationaryFace¶
-
SymmetricBuilder.
StationaryFace
¶ Returns the stationary face.
The constraint is applied between the stationary face and a motion face. The stationary face remains stationary when the constraint is applied.
-------------------------------------
Getter Method
Signature
StationaryFace()
Returns: Return type: NXOpen.SelectFace
New in version NX6.0.0.
License requirements: None.
SymmetryPlaneOption¶
-
SymmetricBuilder.
SymmetryPlaneOption
¶ Returns or sets the symmetry plane option.
The plane of symmetry is the plane that defines symmetry between the stationary face and the motion face. Either
NXOpen.Features.SymmetricBuilderPlaneOptions.Existing
orNXOpen.Features.SymmetricBuilderPlaneOptions.New
plane option could be employed to define the symmetry plane.-------------------------------------
Getter Method
Signature
SymmetryPlaneOption()
Returns: Return type: NXOpen.Features.SymmetricBuilderPlaneOptions
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SymmetryPlaneOption(symmetryPlaneOption)
Parameters: symmetryPlaneOption ( NXOpen.Features.SymmetricBuilderPlaneOptions
) –New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
Method Detail¶
Validate¶
-
SymmetricBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.