FaceRecognitionBuilder Class

class NXOpen.Features.FaceRecognitionBuilder

Bases: NXOpen.TaggedObject, NXOpen.GeometricUtilities.IComponentBuilder

Represents a collection of faces and their relationships to other faces in the model

New in version NX6.0.0.

Properties

Property Description
CoaxialEnabled Returns or sets a value that indicates whether coaxial relation recognition is enabled
CoplanarAxesEnabled Returns or sets a value that indicates whether coplanar axes relation recognition is enabled
CoplanarEnabled Returns or sets a value that indicates whether coplanar relation recognition is enabled
EqualDiameterEnabled Returns or sets a value that indicates whether equal diameter recognition is enabled
FaceCollector Returns the face collector
OffsetEnabled Returns or sets a value that indicates whether symmetric relation recognition is enabled
ParallelEnabled Returns or sets a value that indicates whether parallel relation recognition is enabled
PerpendicularEnabled Returns or sets a value that indicates whether perpendicular relation recognition is enabled
ReferenceCoordinateSystem Returns the reference coordinate system to use for symmetry and coplanar axis recognition
RelationScope Returns or sets a value that indicates what kind of relations are needed to recognize
SymmetricEnabled Returns or sets a value that indicates whether symmetric relation recognition is enabled
Tag Returns the Tag for this object.
TangentEnabled Returns or sets a value that indicates whether tangent relation recognition is enabled
ThicknessChainEnabled Returns or sets a value that indicates whether thickness chain relation recognition is enabled
UseFaceBrowse Returns or sets a value that indicates whether relations are found when faces are added to the face collector

Methods

Method Description
DeleteConstraint Deletes the persistent constraint
DeleteOffsetRelation Deletes the offset relation
DeselectEntities Removes entities from collector
LockConstraint Locks the persistent constraint
RecognizeCoaxial Recognizes coaxial relations to last faces added to face collector
RecognizeCoplanar Recognizes coplanar relations to last faces added to face collector
RecognizeCoplanarAxes Recognizes coplanar axes relations to last faces added to face collector
RecognizeEqualDiameter Recognizes equal diameter relations to last faces added to face collector
RecognizeOffset Recognizes offset relations to last faces added to face collector
RecognizeParallel Recognizes parallel relations to last faces added to face collector
RecognizePerpendicular Recognizes perpendicular relations to last faces added to face collector
RecognizeSymmetric Recognizes symmetric relations to last faces added to face collector
RecognizeTangent Recognizes tangent relations to last faces added to face collector
RecognizeThicknessChain Recognizes thickness chain relations to last faces added to face collector
ReplaceRules Replace collector rules.
SelectEntities Adds entities to collector
UnlockConstraint Unlocks the persistent constraint
UnrecognizeCoaxial Removes coaxial relations to last faces added to face collector
UnrecognizeCoplanar Removes coplanar relations to last faces added to face collector
UnrecognizeCoplanarAxes Removes coplanar axes relations to last faces added to face collector
UnrecognizeEqualDiameter Removes equal diameter relations to last faces added to face collector
UnrecognizeOffset Removes offset relations to last faces added to face collector
UnrecognizeParallel Removes parallel relations to last faces added to face collector
UnrecognizePerpendicular Removes perpendicular relations to last faces added to face collector
UnrecognizeSymmetric Removes symmetric relations to last faces added to face collector
UnrecognizeTangent Removes tangent relations to last faces added to face collector
UnrecognizeThicknessChain Removes thickness chain relations to last faces added to face collector
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Property Detail

CoaxialEnabled

FaceRecognitionBuilder.CoaxialEnabled

Returns or sets a value that indicates whether coaxial relation recognition is enabled

-------------------------------------

Getter Method

Signature CoaxialEnabled()

Returns:
Return type:bool

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature CoaxialEnabled(coaxialEnabled)

Parameters:coaxialEnabled (bool) –

New in version NX6.0.0.

License requirements: gateway (“UG GATEWAY”)

CoplanarAxesEnabled

FaceRecognitionBuilder.CoplanarAxesEnabled

Returns or sets a value that indicates whether coplanar axes relation recognition is enabled

-------------------------------------

Getter Method

Signature CoplanarAxesEnabled()

Returns:
Return type:bool

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature CoplanarAxesEnabled(coplanarEnabled)

Parameters:coplanarEnabled (bool) –

New in version NX6.0.0.

License requirements: gateway (“UG GATEWAY”)

CoplanarEnabled

FaceRecognitionBuilder.CoplanarEnabled

Returns or sets a value that indicates whether coplanar relation recognition is enabled

-------------------------------------

Getter Method

Signature CoplanarEnabled()

Returns:
Return type:bool

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature CoplanarEnabled(coplanarEnabled)

Parameters:coplanarEnabled (bool) –

New in version NX6.0.0.

License requirements: gateway (“UG GATEWAY”)

EqualDiameterEnabled

FaceRecognitionBuilder.EqualDiameterEnabled

Returns or sets a value that indicates whether equal diameter recognition is enabled

-------------------------------------

Getter Method

Signature EqualDiameterEnabled()

Returns:
Return type:bool

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature EqualDiameterEnabled(equalDiameterEnabled)

Parameters:equalDiameterEnabled (bool) –

New in version NX6.0.0.

License requirements: gateway (“UG GATEWAY”)

FaceCollector

FaceRecognitionBuilder.FaceCollector

Returns the face collector

-------------------------------------

Getter Method

Signature FaceCollector()

Returns:
Return type:NXOpen.ScCollector

New in version NX6.0.0.

License requirements: None.

OffsetEnabled

FaceRecognitionBuilder.OffsetEnabled

Returns or sets a value that indicates whether symmetric relation recognition is enabled

-------------------------------------

Getter Method

Signature OffsetEnabled()

Returns:
Return type:bool

New in version NX7.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature OffsetEnabled(offsetEnabled)

Parameters:offsetEnabled (bool) –

New in version NX7.0.0.

License requirements: gateway (“UG GATEWAY”)

ParallelEnabled

FaceRecognitionBuilder.ParallelEnabled

Returns or sets a value that indicates whether parallel relation recognition is enabled

-------------------------------------

Getter Method

Signature ParallelEnabled()

Returns:
Return type:bool

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ParallelEnabled(parallelEnabled)

Parameters:parallelEnabled (bool) –

New in version NX6.0.0.

License requirements: gateway (“UG GATEWAY”)

PerpendicularEnabled

FaceRecognitionBuilder.PerpendicularEnabled

Returns or sets a value that indicates whether perpendicular relation recognition is enabled

-------------------------------------

Getter Method

Signature PerpendicularEnabled()

Returns:
Return type:bool

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature PerpendicularEnabled(perpendicularEnabled)

Parameters:perpendicularEnabled (bool) –

New in version NX6.0.0.

License requirements: gateway (“UG GATEWAY”)

ReferenceCoordinateSystem

FaceRecognitionBuilder.ReferenceCoordinateSystem

Returns the reference coordinate system to use for symmetry and coplanar axis recognition

-------------------------------------

Getter Method

Signature ReferenceCoordinateSystem()

Returns:
Return type:NXOpen.GeometricUtilities.OrientXpressBuilder

New in version NX6.0.0.

License requirements: None.

RelationScope

FaceRecognitionBuilder.RelationScope

Returns or sets a value that indicates what kind of relations are needed to recognize

-------------------------------------

Getter Method

Signature RelationScope()

Returns:
Return type:int

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature RelationScope(relationScope)

Parameters:relationScope (int) –

New in version NX7.5.0.

License requirements: gateway (“UG GATEWAY”)

SymmetricEnabled

FaceRecognitionBuilder.SymmetricEnabled

Returns or sets a value that indicates whether symmetric relation recognition is enabled

-------------------------------------

Getter Method

Signature SymmetricEnabled()

Returns:
Return type:bool

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature SymmetricEnabled(symmetricEnabled)

Parameters:symmetricEnabled (bool) –

New in version NX6.0.0.

License requirements: gateway (“UG GATEWAY”)

TangentEnabled

FaceRecognitionBuilder.TangentEnabled

Returns or sets a value that indicates whether tangent relation recognition is enabled

-------------------------------------

Getter Method

Signature TangentEnabled()

Returns:
Return type:bool

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature TangentEnabled(tangentEnabled)

Parameters:tangentEnabled (bool) –

New in version NX6.0.0.

License requirements: gateway (“UG GATEWAY”)

ThicknessChainEnabled

FaceRecognitionBuilder.ThicknessChainEnabled

Returns or sets a value that indicates whether thickness chain relation recognition is enabled

-------------------------------------

Getter Method

Signature ThicknessChainEnabled()

Returns:
Return type:bool

New in version NX7.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ThicknessChainEnabled(thicknessChainEnabled)

Parameters:thicknessChainEnabled (bool) –

New in version NX7.0.0.

License requirements: gateway (“UG GATEWAY”)

UseFaceBrowse

FaceRecognitionBuilder.UseFaceBrowse

Returns or sets a value that indicates whether relations are found when faces are added to the face collector

-------------------------------------

Getter Method

Signature UseFaceBrowse()

Returns:
Return type:bool

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature UseFaceBrowse(useFaceBrowse)

Parameters:useFaceBrowse (bool) –

New in version NX6.0.0.

License requirements: gateway (“UG GATEWAY”)

Method Detail

DeleteConstraint

FaceRecognitionBuilder.DeleteConstraint

Deletes the persistent constraint

Signature DeleteConstraint(feature)

Parameters:feature (NXOpen.Features.Feature) – the persistent constraint feature

New in version NX7.0.0.

License requirements: gateway (“UG GATEWAY”)

DeleteOffsetRelation

FaceRecognitionBuilder.DeleteOffsetRelation

Deletes the offset relation

Signature DeleteOffsetRelation(offsetFaces)

Parameters:offsetFaces (list of NXOpen.NXObject) –

New in version NX7.0.0.

License requirements: gateway (“UG GATEWAY”)

DeselectEntities

FaceRecognitionBuilder.DeselectEntities

Removes entities from collector

Signature DeselectEntities(entities)

Parameters:entities (list of NXOpen.NXObject) –

New in version NX6.0.0.

License requirements: gateway (“UG GATEWAY”)

LockConstraint

FaceRecognitionBuilder.LockConstraint

Locks the persistent constraint

Signature LockConstraint(feature)

Parameters:feature (NXOpen.Features.Feature) – the persistent constraint feature

New in version NX7.0.0.

License requirements: gateway (“UG GATEWAY”)

RecognizeCoaxial

FaceRecognitionBuilder.RecognizeCoaxial

Recognizes coaxial relations to last faces added to face collector

Signature RecognizeCoaxial(isNear)

Parameters:isNear (bool) – true for near relations, false for far relations

New in version NX6.0.0.

License requirements: gateway (“UG GATEWAY”)

RecognizeCoplanar

FaceRecognitionBuilder.RecognizeCoplanar

Recognizes coplanar relations to last faces added to face collector

Signature RecognizeCoplanar(isNear)

Parameters:isNear (bool) – true for near relations, false for far relations

New in version NX6.0.0.

License requirements: gateway (“UG GATEWAY”)

RecognizeCoplanarAxes

FaceRecognitionBuilder.RecognizeCoplanarAxes

Recognizes coplanar axes relations to last faces added to face collector

Signature RecognizeCoplanarAxes(isNear)

Parameters:isNear (bool) – true for near relations, false for far relations

New in version NX6.0.0.

License requirements: gateway (“UG GATEWAY”)

RecognizeEqualDiameter

FaceRecognitionBuilder.RecognizeEqualDiameter

Recognizes equal diameter relations to last faces added to face collector

Signature RecognizeEqualDiameter(isNear)

Parameters:isNear (bool) – true for near relations, false for far relations

New in version NX6.0.0.

License requirements: gateway (“UG GATEWAY”)

RecognizeOffset

FaceRecognitionBuilder.RecognizeOffset

Recognizes offset relations to last faces added to face collector

Signature RecognizeOffset(isNear)

Parameters:isNear (bool) – true for near relations, false for far relations

New in version NX6.0.0.

License requirements: gateway (“UG GATEWAY”)

RecognizeParallel

FaceRecognitionBuilder.RecognizeParallel

Recognizes parallel relations to last faces added to face collector

Signature RecognizeParallel(isNear)

Parameters:isNear (bool) – true for near relations, false for far relations

New in version NX6.0.0.

License requirements: gateway (“UG GATEWAY”)

RecognizePerpendicular

FaceRecognitionBuilder.RecognizePerpendicular

Recognizes perpendicular relations to last faces added to face collector

Signature RecognizePerpendicular(isNear)

Parameters:isNear (bool) – true for near relations, false for far relations

New in version NX6.0.0.

License requirements: gateway (“UG GATEWAY”)

RecognizeSymmetric

FaceRecognitionBuilder.RecognizeSymmetric

Recognizes symmetric relations to last faces added to face collector

Signature RecognizeSymmetric(isNear)

Parameters:isNear (bool) – true for near relations, false for far relations

New in version NX6.0.0.

License requirements: gateway (“UG GATEWAY”)

RecognizeTangent

FaceRecognitionBuilder.RecognizeTangent

Recognizes tangent relations to last faces added to face collector

Signature RecognizeTangent(isNear)

Parameters:isNear (bool) – true for near relations, false for far relations

New in version NX6.0.0.

License requirements: gateway (“UG GATEWAY”)

RecognizeThicknessChain

FaceRecognitionBuilder.RecognizeThicknessChain

Recognizes thickness chain relations to last faces added to face collector

Signature RecognizeThicknessChain(isNear)

Parameters:isNear (bool) – true for near relations, false for far relations

New in version NX7.0.0.

License requirements: gateway (“UG GATEWAY”)

ReplaceRules

FaceRecognitionBuilder.ReplaceRules

Replace collector rules.

Signature ReplaceRules(rules, createRulesWoUpdate)

Parameters:
  • rules (list of NXOpen.SelectionIntentRule) – Selection intent rules. To create selection intent rules see documentation of ScRuleFactory for more details.
  • createRulesWoUpdate (bool) – Flag to tell whether rules should be created wo_update

New in version NX7.0.0.

License requirements: gateway (“UG GATEWAY”)

SelectEntities

FaceRecognitionBuilder.SelectEntities

Adds entities to collector

Signature SelectEntities(entities)

Parameters:entities (list of NXOpen.NXObject) –

New in version NX6.0.0.

License requirements: gateway (“UG GATEWAY”)

UnlockConstraint

FaceRecognitionBuilder.UnlockConstraint

Unlocks the persistent constraint

Signature UnlockConstraint(feature)

Parameters:feature (NXOpen.Features.Feature) – the persistent constraint feature

New in version NX7.0.0.

License requirements: gateway (“UG GATEWAY”)

UnrecognizeCoaxial

FaceRecognitionBuilder.UnrecognizeCoaxial

Removes coaxial relations to last faces added to face collector

Signature UnrecognizeCoaxial(isNear)

Parameters:isNear (bool) – true for near relations, false for far relations

New in version NX6.0.0.

License requirements: gateway (“UG GATEWAY”)

UnrecognizeCoplanar

FaceRecognitionBuilder.UnrecognizeCoplanar

Removes coplanar relations to last faces added to face collector

Signature UnrecognizeCoplanar(isNear)

Parameters:isNear (bool) – true for near relations, false for far relations

New in version NX6.0.0.

License requirements: gateway (“UG GATEWAY”)

UnrecognizeCoplanarAxes

FaceRecognitionBuilder.UnrecognizeCoplanarAxes

Removes coplanar axes relations to last faces added to face collector

Signature UnrecognizeCoplanarAxes(isNear)

Parameters:isNear (bool) – true for near relations, false for far relations

New in version NX6.0.0.

License requirements: gateway (“UG GATEWAY”)

UnrecognizeEqualDiameter

FaceRecognitionBuilder.UnrecognizeEqualDiameter

Removes equal diameter relations to last faces added to face collector

Signature UnrecognizeEqualDiameter(isNear)

Parameters:isNear (bool) – true for near relations, false for far relations

New in version NX6.0.0.

License requirements: gateway (“UG GATEWAY”)

UnrecognizeOffset

FaceRecognitionBuilder.UnrecognizeOffset

Removes offset relations to last faces added to face collector

Signature UnrecognizeOffset(isNear)

Parameters:isNear (bool) – true for near relations, false for far relations

New in version NX6.0.0.

License requirements: gateway (“UG GATEWAY”)

UnrecognizeParallel

FaceRecognitionBuilder.UnrecognizeParallel

Removes parallel relations to last faces added to face collector

Signature UnrecognizeParallel(isNear)

Parameters:isNear (bool) – true for near relations, false for far relations

New in version NX6.0.0.

License requirements: gateway (“UG GATEWAY”)

UnrecognizePerpendicular

FaceRecognitionBuilder.UnrecognizePerpendicular

Removes perpendicular relations to last faces added to face collector

Signature UnrecognizePerpendicular(isNear)

Parameters:isNear (bool) – true for near relations, false for far relations

New in version NX6.0.0.

License requirements: gateway (“UG GATEWAY”)

UnrecognizeSymmetric

FaceRecognitionBuilder.UnrecognizeSymmetric

Removes symmetric relations to last faces added to face collector

Signature UnrecognizeSymmetric(isNear)

Parameters:isNear (bool) – true for near relations, false for far relations

New in version NX6.0.0.

License requirements: gateway (“UG GATEWAY”)

UnrecognizeTangent

FaceRecognitionBuilder.UnrecognizeTangent

Removes tangent relations to last faces added to face collector

Signature UnrecognizeTangent(isNear)

Parameters:isNear (bool) – true for near relations, false for far relations

New in version NX6.0.0.

License requirements: gateway (“UG GATEWAY”)

UnrecognizeThicknessChain

FaceRecognitionBuilder.UnrecognizeThicknessChain

Removes thickness chain relations to last faces added to face collector

Signature UnrecognizeThicknessChain(isNear)

Parameters:isNear (bool) – true for near relations, false for far relations

New in version NX7.0.0.

License requirements: gateway (“UG GATEWAY”)

Validate

FaceRecognitionBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.