SubdivisionSplitFaceBuilder Class¶
-
class
NXOpen.Features.Subdivision.
SubdivisionSplitFaceBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Features.Subdivision.SubdivisionSplitFaceBuilder
builder.To create a new instance of this class, use
NXOpen.Features.Subdivision.SubdivisionBodyCollection.CreateSubdivisionSplitFaceBuilder()
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
FacesToSplit | Returns the faces to split. |
Number | Returns or sets the desired split number in one face. |
ReferenceEdge | Returns the reference edges. |
Tag | Returns the Tag for this object. |
Type | Returns or sets the split type. |
Methods¶
Method | Description |
---|---|
AddSplitPoint | Add split face point. |
ClearSplitPoints | Clear split face point. |
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UpdateSplitPositions | Update split positions. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
SubdivisionSplitFaceBuilderTypes Enumeration | Represents the split type. |
Property Detail¶
FacesToSplit¶
-
SubdivisionSplitFaceBuilder.
FacesToSplit
¶ Returns the faces to split.
-------------------------------------
Getter Method
Signature
FacesToSplit()
Returns: Return type: NXOpen.Features.Subdivision.SelectCageObjectData
New in version NX9.0.0.
License requirements: None.
Number¶
-
SubdivisionSplitFaceBuilder.
Number
¶ Returns or sets the desired split number in one face.
-------------------------------------
Getter Method
Signature
Number()
Returns: Return type: int New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Number(number)
Parameters: number (int) – New in version NX9.0.0.
License requirements: nx_subdivision (” NX SUBDIVISION”)
ReferenceEdge¶
-
SubdivisionSplitFaceBuilder.
ReferenceEdge
¶ Returns the reference edges.
-------------------------------------
Getter Method
Signature
ReferenceEdge()
Returns: Return type: NXOpen.Features.Subdivision.SelectCageObjectData
New in version NX9.0.0.
License requirements: None.
Type¶
-
SubdivisionSplitFaceBuilder.
Type
¶ Returns or sets the split type.
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.Features.Subdivision.SubdivisionSplitFaceBuilderTypes
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(type)
Parameters: type ( NXOpen.Features.Subdivision.SubdivisionSplitFaceBuilderTypes
) –New in version NX9.0.0.
License requirements: nx_subdivision (” NX SUBDIVISION”)
Method Detail¶
AddSplitPoint¶
-
SubdivisionSplitFaceBuilder.
AddSplitPoint
¶ Add split face point.
Signature
AddSplitPoint(location, object)
Parameters: - location (
NXOpen.Point3d
) – the loction on the object to split face. - object (
NXOpen.DisplayableObject
) – the selected subdivision edge or vertex to split face.
New in version NX9.0.0.
License requirements: nx_subdivision (” NX SUBDIVISION”)
- location (
ClearSplitPoints¶
-
SubdivisionSplitFaceBuilder.
ClearSplitPoints
¶ Clear split face point.
Signature
ClearSplitPoints()
New in version NX10.0.0.
License requirements: nx_subdivision (” NX SUBDIVISION”)
UpdateSplitPositions¶
-
SubdivisionSplitFaceBuilder.
UpdateSplitPositions
¶ Update split positions.
Signature
UpdateSplitPositions(splitLineIndex, positions)
Parameters: - splitLineIndex (int) – index to indicate which split line to update positions from.
- positions (list of
NXOpen.Point3d
) – the point positions.
New in version NX10.0.0.
License requirements: nx_subdivision (” NX SUBDIVISION”)
Validate¶
-
SubdivisionSplitFaceBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.