SubdivisionSplitFaceBuilderTypes Enumeration

NXOpen.Features.Subdivision.SubdivisionSplitFaceBuilder.Types is an alias for NXOpen.Features.Subdivision.SubdivisionSplitFaceBuilderTypes

class NXOpen.Features.Subdivision.SubdivisionSplitFaceBuilderTypes

Bases: object

Represents the split type.

Enum Members

Enum Member Enum Member Description
Uniform
Uniform split type.
ThroughLines
Through lines split type.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.