TraceLinesBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
TraceLinesBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.ShipDesign.TraceLines
builderTo create a new instance of this class, use
NXOpen.Features.ShipCollection.CreateTraceLinesBuilder()
Default values.
Property Value Associative 1 CurveCount 1 Offset.Value 0 (millimeters part), 0 (inches part) OffsetCurveCount 1 OffsetType EqualSpacing New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
Associative | Returns or sets the associative |
CurveCount | Returns or sets the curve count |
DatumPlanes | Returns the datum planes |
Direction | Returns or sets the direction |
EndCurve | Returns the end curve |
Offset | Returns the offset |
OffsetCurveCount | Returns or sets the offset curve count |
OffsetType | Returns or sets the offset type |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
PlacementFace | Returns the placement face |
ReferenceCurve | Returns the reference curve |
StartCurve | Returns the start curve |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
TraceLinesBuilderTraceLineType Enumeration | Define the traceline creation method |
Property Detail¶
Associative¶
-
TraceLinesBuilder.
Associative
¶ Returns or sets the associative
-------------------------------------
Getter Method
Signature
Associative()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Associative(associative)
Parameters: associative (bool) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”)
CurveCount¶
-
TraceLinesBuilder.
CurveCount
¶ Returns or sets the curve count
-------------------------------------
Getter Method
Signature
CurveCount()
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CurveCount(curveCount)
Parameters: curveCount (int) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”)
DatumPlanes¶
-
TraceLinesBuilder.
DatumPlanes
¶ Returns the datum planes
-------------------------------------
Getter Method
Signature
DatumPlanes()
Returns: Return type: NXOpen.SelectDisplayableObjectList
New in version NX7.5.0.
License requirements: None.
Direction¶
-
TraceLinesBuilder.
Direction
¶ Returns or sets the direction
-------------------------------------
Getter Method
Signature
Direction()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Direction(direction)
Parameters: direction (bool) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”)
EndCurve¶
-
TraceLinesBuilder.
EndCurve
¶ Returns the end curve
-------------------------------------
Getter Method
Signature
EndCurve()
Returns: Return type: NXOpen.Section
New in version NX7.5.0.
License requirements: None.
Offset¶
-
TraceLinesBuilder.
Offset
¶ Returns the offset
-------------------------------------
Getter Method
Signature
Offset()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
OffsetCurveCount¶
-
TraceLinesBuilder.
OffsetCurveCount
¶ Returns or sets the offset curve count
-------------------------------------
Getter Method
Signature
OffsetCurveCount()
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OffsetCurveCount(offsetCurveCount)
Parameters: offsetCurveCount (int) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”)
OffsetType¶
-
TraceLinesBuilder.
OffsetType
¶ Returns or sets the offset type
-------------------------------------
Getter Method
Signature
OffsetType()
Returns: Return type: NXOpen.Features.ShipDesign.TraceLinesBuilderTraceLineType
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OffsetType(offsetType)
Parameters: offsetType ( NXOpen.Features.ShipDesign.TraceLinesBuilderTraceLineType
) –New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”)
PlacementFace¶
-
TraceLinesBuilder.
PlacementFace
¶ Returns the placement face
-------------------------------------
Getter Method
Signature
PlacementFace()
Returns: Return type: NXOpen.ScCollector
New in version NX7.5.0.
License requirements: None.
ReferenceCurve¶
-
TraceLinesBuilder.
ReferenceCurve
¶ Returns the reference curve
-------------------------------------
Getter Method
Signature
ReferenceCurve()
Returns: Return type: NXOpen.Section
New in version NX7.5.0.
License requirements: None.
StartCurve¶
-
TraceLinesBuilder.
StartCurve
¶ Returns the start curve
-------------------------------------
Getter Method
Signature
StartCurve()
Returns: Return type: NXOpen.Section
New in version NX7.5.0.
License requirements: None.
Method Detail¶
Validate¶
-
TraceLinesBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.