ShellExpansionBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
ShellExpansionBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.ShipDesign.ShellExpansion
builderTo create a new instance of this class, use
NXOpen.Features.ShipCollection.CreateShellExpansionBuilder()
Default values.
Property Value AdditionalPlanesPerFrame 0 Associative 1 MapFaceEdges 1 MapTransverseFrames 1 Tolerance 1.0 New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
AdditionalPlanesPerFrame | Returns or sets the additional planes per frame |
AftLimitPlane | Returns the aft limit plane |
Associative | Returns or sets a flag that determines if output is associative (only used during creation). |
BasePlane | Returns the base plane |
CurvesToMap | Returns the curves to map |
FacesToFlatten | Returns the faces to flatten |
ForeLimitPlane | Returns the fore limit plane |
MapFaceEdges | Returns or sets the map face edges |
MapTransverseFrames | Returns or sets the map transverse frames |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Tolerance | Returns or sets the tolerance |
UpperLimitPlane | Returns the upper limit plane |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AdditionalPlanesPerFrame¶
-
ShellExpansionBuilder.
AdditionalPlanesPerFrame
¶ Returns or sets the additional planes per frame
-------------------------------------
Getter Method
Signature
AdditionalPlanesPerFrame()
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AdditionalPlanesPerFrame(additionalPlanesPerFrame)
Parameters: additionalPlanesPerFrame (int) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”)
AftLimitPlane¶
-
ShellExpansionBuilder.
AftLimitPlane
¶ Returns the aft limit plane
-------------------------------------
Getter Method
Signature
AftLimitPlane()
Returns: Return type: NXOpen.SelectDatumPlane
New in version NX7.5.0.
License requirements: None.
Associative¶
-
ShellExpansionBuilder.
Associative
¶ Returns or sets a flag that determines if output is associative (only used during creation).
-------------------------------------
Getter Method
Signature
Associative()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Associative(associative)
Parameters: associative (bool) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”)
BasePlane¶
-
ShellExpansionBuilder.
BasePlane
¶ Returns the base plane
-------------------------------------
Getter Method
Signature
BasePlane()
Returns: Return type: NXOpen.SelectDatumPlane
New in version NX7.5.0.
License requirements: None.
CurvesToMap¶
-
ShellExpansionBuilder.
CurvesToMap
¶ Returns the curves to map
-------------------------------------
Getter Method
Signature
CurvesToMap()
Returns: Return type: NXOpen.Section
New in version NX7.5.0.
License requirements: None.
FacesToFlatten¶
-
ShellExpansionBuilder.
FacesToFlatten
¶ Returns the faces to flatten
-------------------------------------
Getter Method
Signature
FacesToFlatten()
Returns: Return type: NXOpen.ScCollector
New in version NX7.5.0.
License requirements: None.
ForeLimitPlane¶
-
ShellExpansionBuilder.
ForeLimitPlane
¶ Returns the fore limit plane
-------------------------------------
Getter Method
Signature
ForeLimitPlane()
Returns: Return type: NXOpen.SelectDatumPlane
New in version NX7.5.0.
License requirements: None.
MapFaceEdges¶
-
ShellExpansionBuilder.
MapFaceEdges
¶ Returns or sets the map face edges
-------------------------------------
Getter Method
Signature
MapFaceEdges()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MapFaceEdges(mapFaceEdges)
Parameters: mapFaceEdges (bool) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”)
MapTransverseFrames¶
-
ShellExpansionBuilder.
MapTransverseFrames
¶ Returns or sets the map transverse frames
-------------------------------------
Getter Method
Signature
MapTransverseFrames()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MapTransverseFrames(mapTransverseFrames)
Parameters: mapTransverseFrames (bool) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”)
Tolerance¶
-
ShellExpansionBuilder.
Tolerance
¶ Returns or sets the tolerance
-------------------------------------
Getter Method
Signature
Tolerance()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Tolerance(tolerance)
Parameters: tolerance (float) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”)
UpperLimitPlane¶
-
ShellExpansionBuilder.
UpperLimitPlane
¶ Returns the upper limit plane
-------------------------------------
Getter Method
Signature
UpperLimitPlane()
Returns: Return type: NXOpen.SelectDatumPlane
New in version NX7.5.0.
License requirements: None.
Method Detail¶
Validate¶
-
ShellExpansionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.