PlateBoundaryOptionBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
PlateBoundaryOptionBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Features.ShipDesign.PlateBoundaryOptionBuilder
builder to define the plate boundary option.This builder returns None.
To create a new instance of this class, use
NXOpen.Features.ShipDesign.PlateBuilder.CreatePlateBoundaryOptionBuilder()
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
BoundaryType | Returns or sets the plate boundary types. |
Tag | Returns the Tag for this object. |
TrimType | Returns or sets the plate boundary trim types. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
PlateBoundaryOptionBuilderBoundaryTypes Enumeration |
|
PlateBoundaryOptionBuilderTrimTypes Enumeration |
|
Property Detail¶
BoundaryType¶
-
PlateBoundaryOptionBuilder.
BoundaryType
¶ Returns or sets the plate boundary types.
-------------------------------------
Getter Method
Signature
BoundaryType()
Returns: Return type: NXOpen.Features.ShipDesign.PlateBoundaryOptionBuilderBoundaryTypes
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BoundaryType(boundaryType)
Parameters: boundaryType ( NXOpen.Features.ShipDesign.PlateBoundaryOptionBuilderBoundaryTypes
) –New in version NX11.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
TrimType¶
-
PlateBoundaryOptionBuilder.
TrimType
¶ Returns or sets the plate boundary trim types.
-------------------------------------
Getter Method
Signature
TrimType()
Returns: Return type: NXOpen.Features.ShipDesign.PlateBoundaryOptionBuilderTrimTypes
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TrimType(trimType)
Parameters: trimType ( NXOpen.Features.ShipDesign.PlateBoundaryOptionBuilderTrimTypes
) –New in version NX11.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
Method Detail¶
Validate¶
-
PlateBoundaryOptionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.