PlateBoundaryOptionBuilderBoundaryTypes Enumeration¶
NXOpen.Features.ShipDesign.PlateBoundaryOptionBuilder.BoundaryTypes is an alias for NXOpen.Features.ShipDesign.PlateBoundaryOptionBuilderBoundaryTypes
-
class
NXOpen.Features.ShipDesign.
PlateBoundaryOptionBuilderBoundaryTypes
¶ Bases:
object
The plate boundary types.
This option specifies the plate boundary object type. Different boundary object type may have different
NXOpen.Features.ShipDesign.PlateBoundaryOptionBuilderTrimTypes
.Enum Members
Enum Member Enum Member Description Curve useNXOpen.Curve
as the boundary.Solid useNXOpen.Body
as the boundary.FacePlane useNXOpen.Face
orNXOpen.Plane
as the boundary.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-