ManufacturingOutBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
ManufacturingOutBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.ShipDesign.ManufacturingOut
builderTo create a new instance of this class, use
NXOpen.Features.ShipCollection.CreateManufacturingOutBuilder()
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
Component | Returns the component to validate |
ConfigFile | Returns or sets the XML confiuration file |
MarkOnlySection | Returns the mark only section |
OutputFile | Returns or sets the output spreadsheet file |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Component¶
-
ManufacturingOutBuilder.
Component
¶ Returns the component to validate
-------------------------------------
Getter Method
Signature
Component()
Returns: Return type: NXOpen.SelectDisplayableObject
New in version NX9.0.2.
License requirements: None.
ConfigFile¶
-
ManufacturingOutBuilder.
ConfigFile
¶ Returns or sets the XML confiuration file
-------------------------------------
Getter Method
Signature
ConfigFile()
Returns: Return type: str New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ConfigFile(fileName)
Parameters: fileName (str) – New in version NX5.0.0.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_mfg_prep (“Ship Manufacturing”)
MarkOnlySection¶
-
ManufacturingOutBuilder.
MarkOnlySection
¶ Returns the mark only section
-------------------------------------
Getter Method
Signature
MarkOnlySection()
Returns: Return type: NXOpen.Section
New in version NX9.0.2.
License requirements: None.
OutputFile¶
-
ManufacturingOutBuilder.
OutputFile
¶ Returns or sets the output spreadsheet file
-------------------------------------
Getter Method
Signature
OutputFile()
Returns: Return type: str New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OutputFile(fileName)
Parameters: fileName (str) – New in version NX5.0.0.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_mfg_prep (“Ship Manufacturing”)
Method Detail¶
Validate¶
-
ManufacturingOutBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.