LouverBuilder Class¶
-
class
NXOpen.Features.SheetMetal.
LouverBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a louver feature builder.
To create a new instance of this class, use
NXOpen.Features.SheetMetal.SheetmetalManager.CreateLouverFeatureBuilder()
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
Depth | Returns the depth of the louver |
DepthSide | Returns or sets the depth side for the louver. |
DieRadius | Returns the die radius. |
EndType | Returns or sets the end type for the louver. |
IncludeRounding | Returns or sets the option to round the edges of the louver using the die radius. |
MinimumToolClearance | Returns the minimum tool clearance expression. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
Section | Returns or sets the section used by the louver. |
SectionSide | Returns or sets the side of the section on which the louver is created and width is measure. |
Sketch | Returns or sets the internal sketch used by the louver’s section. |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Width | Returns the width of the louver. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetDepth | |
SetDieRadius | |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
SetWidth | |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
ValidateBuilderData | This method verifies that the builder data is valid for louver creation. |
Enumerations¶
LouverBuilderDepthSideOptions Enumeration | This enum represents the depth side for the louver. |
LouverBuilderEndTypeOptions Enumeration | This enum represents the end type for the louver. |
LouverBuilderSectionSideOptions Enumeration | This enum represents the side of the section that the louver width is measured. |
Property Detail¶
Depth¶
-
LouverBuilder.
Depth
¶ Returns the depth of the louver
-------------------------------------
Getter Method
Signature
Depth()
Returns: The depth of the louver Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
DepthSide¶
-
LouverBuilder.
DepthSide
¶ Returns or sets the depth side for the louver.
-------------------------------------
Getter Method
Signature
DepthSide()
Returns: Return type: NXOpen.Features.SheetMetal.LouverBuilderDepthSideOptions
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
-------------------------------------
Setter Method
Signature
DepthSide(depthSide)
Parameters: depthSide ( NXOpen.Features.SheetMetal.LouverBuilderDepthSideOptions
) –New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
DieRadius¶
-
LouverBuilder.
DieRadius
¶ Returns the die radius.
Not used if
NXOpen.Features.SheetMetal.LouverBuilder.IncludeRounding()
is false.-------------------------------------
Getter Method
Signature
DieRadius()
Returns: Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
EndType¶
-
LouverBuilder.
EndType
¶ Returns or sets the end type for the louver.
Select lanced end or formed end from
NXOpen.Features.SheetMetal.LouverBuilderEndTypeOptions
.-------------------------------------
Getter Method
Signature
EndType()
Returns: Return type: NXOpen.Features.SheetMetal.LouverBuilderEndTypeOptions
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
-------------------------------------
Setter Method
Signature
EndType(endType)
Parameters: endType ( NXOpen.Features.SheetMetal.LouverBuilderEndTypeOptions
) –New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
IncludeRounding¶
-
LouverBuilder.
IncludeRounding
¶ Returns or sets the option to round the edges of the louver using the die radius.
If this is false, then the value of
NXOpen.Features.SheetMetal.LouverBuilder.DieRadius()
is not used.-------------------------------------
Getter Method
Signature
IncludeRounding()
Returns: Return type: bool New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
-------------------------------------
Setter Method
Signature
IncludeRounding(includeRounding)
Parameters: includeRounding (bool) – New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
MinimumToolClearance¶
-
LouverBuilder.
MinimumToolClearance
¶ Returns the minimum tool clearance expression.
-------------------------------------
Getter Method
Signature
MinimumToolClearance()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
Section¶
-
LouverBuilder.
Section
¶ Returns or sets the section used by the louver.
The section should be open.
-------------------------------------
Getter Method
Signature
Section()
Returns: Return type: NXOpen.Section
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
-------------------------------------
Setter Method
Signature
Section(section)
Parameters: section ( NXOpen.Section
) –New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
SectionSide¶
-
LouverBuilder.
SectionSide
¶ Returns or sets the side of the section on which the louver is created and width is measure.
-------------------------------------
Getter Method
Signature
SectionSide()
Returns: Return type: NXOpen.Features.SheetMetal.LouverBuilderSectionSideOptions
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
-------------------------------------
Setter Method
Signature
SectionSide(sectionSide)
Parameters: sectionSide ( NXOpen.Features.SheetMetal.LouverBuilderSectionSideOptions
) –New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
Sketch¶
-
LouverBuilder.
Sketch
¶ Returns or sets the internal sketch used by the louver’s section.
If the sketch is created internally as part of the louver command in the UI, then it is consumed by the louver and does not show up as a separate feature in the part navigator. By setting the sketch object here, you will be making it internal to the louver feature.
-------------------------------------
Getter Method
Signature
Sketch()
Returns: Return type: NXOpen.Features.SketchFeature
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
-------------------------------------
Setter Method
Signature
Sketch(sketch)
Parameters: sketch ( NXOpen.Features.SketchFeature
) –New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
Width¶
-
LouverBuilder.
Width
¶ Returns the width of the louver.
The side of the section that the width is measured from depends on the value of the section side (see
NXOpen.Features.SheetMetal.LouverBuilder.SectionSide()
).-------------------------------------
Getter Method
Signature
Width()
Returns: The width of the louver Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
Method Detail¶
SetDepth¶
-
LouverBuilder.
SetDepth
¶ Signature
SetDepth(depth)
Parameters: depth (str) – New in version NX4.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.Expression.RightHandSide()
on theNXOpen.Expression
object returned fromNXOpen.Features.SheetMetal.LouverBuilder.Depth()
instead.License requirements: nx_sheet_metal (“NX Sheet Metal”)
SetDieRadius¶
-
LouverBuilder.
SetDieRadius
¶ Signature
SetDieRadius(dieRadius)
Parameters: dieRadius (str) – New in version NX4.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.Expression.RightHandSide()
on theNXOpen.Expression
object returned fromNXOpen.Features.SheetMetal.LouverBuilder.DieRadius()
instead.License requirements: nx_sheet_metal (“NX Sheet Metal”)
SetWidth¶
-
LouverBuilder.
SetWidth
¶ Signature
SetWidth(width)
Parameters: width (str) – New in version NX4.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.Expression.RightHandSide()
on theNXOpen.Expression
object returned fromNXOpen.Features.SheetMetal.LouverBuilder.Width()
instead.License requirements: nx_sheet_metal (“NX Sheet Metal”)
Validate¶
-
LouverBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.
ValidateBuilderData¶
-
LouverBuilder.
ValidateBuilderData
¶ This method verifies that the builder data is valid for louver creation.
If the builder data is valid, it returns a value of 0.
Signature
ValidateBuilderData()
Returns: data validity flag Return type: int New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)