LighteningCutoutBuilder Class¶
-
class
NXOpen.Features.SheetMetal.
LighteningCutoutBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
Features.SheetMetal.LighteningCutout
builderTo create a new instance of this class, use
NXOpen.Features.SheetMetal.SheetmetalManager.CreateLighteningCutoutBuilder()
Default values.
Property Value Angle.Value 45 CheckClearance 1 Clearance.Value 5 (millimeters part), 0.12 (inches part) Diameter.Value 102 (millimeters part), 2.6 (inches part) DieRadius.Value 8 (millimeters part), 0.2 (inches part) Length.Value 6 (millimeters part), 0.125 (inches part) NeutralFactor.Value 0.33 SectionCornerRadius.Value 8 (millimeters part), 0.2 (inches part) Type UserDefined New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
Angle | Returns the angle |
CheckClearance | Returns or sets whether to check the clearance |
Clearance | Returns the clearance |
Diameter | Returns the diameter when the type is NXOpen.Features.SheetMetal.LighteningCutoutBuilderCutoutType.Hole |
DieRadius | Returns the die radius |
HoleCenter | Returns the hole center when the type is NXOpen.Features.SheetMetal.LighteningCutoutBuilderCutoutType.Hole |
Length | Returns the length |
NeutralFactor | Returns the neutral factor |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
ReverseBendDirection | Returns or sets whether the bend direction is reversed |
SectionCornerRadius | Returns the section corner radius |
Sketch | Returns the Sketch used by Lightening Cutout |
StandardName | Returns or sets the standard name selected |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Type | Returns or sets the type |
UserDefinedSection | Returns the section when the type is NXOpen.Features.SheetMetal.LighteningCutoutBuilderCutoutType.UserDefined |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
GetStandards | Returns the standard names available for the material selected @return |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
LighteningCutoutBuilderCutoutType Enumeration | Represents the type of Lightening Cutout |
Property Detail¶
Angle¶
-
LighteningCutoutBuilder.
Angle
¶ Returns the angle
-------------------------------------
Getter Method
Signature
Angle()
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: None.
CheckClearance¶
-
LighteningCutoutBuilder.
CheckClearance
¶ Returns or sets whether to check the clearance
-------------------------------------
Getter Method
Signature
CheckClearance()
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CheckClearance(checkClearance)
Parameters: checkClearance (bool) – New in version NX11.0.0.
License requirements: adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
Clearance¶
-
LighteningCutoutBuilder.
Clearance
¶ Returns the clearance
-------------------------------------
Getter Method
Signature
Clearance()
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: None.
Diameter¶
-
LighteningCutoutBuilder.
Diameter
¶ Returns the diameter when the type is
NXOpen.Features.SheetMetal.LighteningCutoutBuilderCutoutType.Hole
-------------------------------------
Getter Method
Signature
Diameter()
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: None.
DieRadius¶
-
LighteningCutoutBuilder.
DieRadius
¶ Returns the die radius
-------------------------------------
Getter Method
Signature
DieRadius()
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: None.
HoleCenter¶
-
LighteningCutoutBuilder.
HoleCenter
¶ Returns the hole center when the type is
NXOpen.Features.SheetMetal.LighteningCutoutBuilderCutoutType.Hole
-------------------------------------
Getter Method
Signature
HoleCenter()
Returns: Return type: NXOpen.Section
New in version NX11.0.0.
License requirements: None.
Length¶
-
LighteningCutoutBuilder.
Length
¶ Returns the length
-------------------------------------
Getter Method
Signature
Length()
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: None.
NeutralFactor¶
-
LighteningCutoutBuilder.
NeutralFactor
¶ Returns the neutral factor
-------------------------------------
Getter Method
Signature
NeutralFactor()
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: None.
ReverseBendDirection¶
-
LighteningCutoutBuilder.
ReverseBendDirection
¶ Returns or sets whether the bend direction is reversed
-------------------------------------
Getter Method
Signature
ReverseBendDirection()
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReverseBendDirection(reverseBendDirection)
Parameters: reverseBendDirection (bool) – New in version NX11.0.0.
License requirements: adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
SectionCornerRadius¶
-
LighteningCutoutBuilder.
SectionCornerRadius
¶ Returns the section corner radius
-------------------------------------
Getter Method
Signature
SectionCornerRadius()
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: None.
Sketch¶
-
LighteningCutoutBuilder.
Sketch
¶ Returns the Sketch used by Lightening Cutout
-------------------------------------
Getter Method
Signature
Sketch()
Returns: Return type: NXOpen.Features.SketchFeature
New in version NX11.0.0.
License requirements: None.
StandardName¶
-
LighteningCutoutBuilder.
StandardName
¶ Returns or sets the standard name selected
-------------------------------------
Getter Method
Signature
StandardName()
Returns: Return type: str New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StandardName(standardName)
Parameters: standardName (str) – New in version NX11.0.0.
License requirements: adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
Type¶
-
LighteningCutoutBuilder.
Type
¶ Returns or sets the type
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.Features.SheetMetal.LighteningCutoutBuilderCutoutType
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(type)
Parameters: type ( NXOpen.Features.SheetMetal.LighteningCutoutBuilderCutoutType
) –New in version NX11.0.0.
License requirements: adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
UserDefinedSection¶
-
LighteningCutoutBuilder.
UserDefinedSection
¶ Returns the section when the type is
NXOpen.Features.SheetMetal.LighteningCutoutBuilderCutoutType.UserDefined
-------------------------------------
Getter Method
Signature
UserDefinedSection()
Returns: Return type: NXOpen.Section
New in version NX11.0.0.
License requirements: None.
Method Detail¶
GetStandards¶
-
LighteningCutoutBuilder.
GetStandards
¶ Returns the standard names available for the material selected
Signature
GetStandards()
Returns: Return type: list of str New in version NX11.0.0.
License requirements: None.
Validate¶
-
LighteningCutoutBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.