JoggleBuilder Class¶
-
class
NXOpen.Features.SheetMetal.
JoggleBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a Sheetmetal joggle builder class.
To create a new instance of this class, use
NXOpen.Features.SheetMetal.SheetmetalManager.CreateJoggleBuilder()
Default values.
Property Value Adjustment.Value 0 FlatPatternCompensation 0 LimitType Single SymmetricSides 1 New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
Adjustment | Returns the adjustment |
EndPlane | Returns or sets the end plane |
FlatPatternCompensation | Returns or sets the flat pattern compensation |
InputList | Returns the input list |
LimitType | Returns or sets the limit type |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
Side1Options | Returns the joggle side 1 options |
Side2Options | Returns the joggle side 2 options |
StartPlane | Returns or sets the start plane |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
SymmetricSides | Returns or sets the symmetric sides |
Tag | Returns the Tag for this object. |
UseMaterialTable | Returns or sets the Use Material Table |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
CreateJoggleInputListItem | Create a input list item. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
JoggleBuilderLimitTypes Enumeration | This enum defines the limit types |
Property Detail¶
Adjustment¶
-
JoggleBuilder.
Adjustment
¶ Returns the adjustment
-------------------------------------
Getter Method
Signature
Adjustment()
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: None.
EndPlane¶
-
JoggleBuilder.
EndPlane
¶ Returns or sets the end plane
-------------------------------------
Getter Method
Signature
EndPlane()
Returns: Return type: NXOpen.Plane
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndPlane(endPlane)
Parameters: endPlane ( NXOpen.Plane
) –New in version NX11.0.0.
License requirements: adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
FlatPatternCompensation¶
-
JoggleBuilder.
FlatPatternCompensation
¶ Returns or sets the flat pattern compensation
-------------------------------------
Getter Method
Signature
FlatPatternCompensation()
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FlatPatternCompensation(flatPatternCompensation)
Parameters: flatPatternCompensation (bool) – New in version NX11.0.0.
License requirements: adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
InputList¶
-
JoggleBuilder.
InputList
¶ Returns the input list
-------------------------------------
Getter Method
Signature
InputList()
Returns: Return type: NXOpen.Features.SheetMetal.JoggleInputListItemBuilderList
New in version NX11.0.0.
License requirements: adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
LimitType¶
-
JoggleBuilder.
LimitType
¶ Returns or sets the limit type
-------------------------------------
Getter Method
Signature
LimitType()
Returns: Return type: NXOpen.Features.SheetMetal.JoggleBuilderLimitTypes
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LimitType(limitType)
Parameters: limitType ( NXOpen.Features.SheetMetal.JoggleBuilderLimitTypes
) –New in version NX11.0.0.
License requirements: adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
Side1Options¶
-
JoggleBuilder.
Side1Options
¶ Returns the joggle side 1 options
-------------------------------------
Getter Method
Signature
Side1Options()
Returns: Return type: NXOpen.Features.SheetMetal.JoggleSideOptionsBuilder
New in version NX11.0.0.
License requirements: adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
Side2Options¶
-
JoggleBuilder.
Side2Options
¶ Returns the joggle side 2 options
-------------------------------------
Getter Method
Signature
Side2Options()
Returns: Return type: NXOpen.Features.SheetMetal.JoggleSideOptionsBuilder
New in version NX11.0.0.
License requirements: adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
StartPlane¶
-
JoggleBuilder.
StartPlane
¶ Returns or sets the start plane
-------------------------------------
Getter Method
Signature
StartPlane()
Returns: Return type: NXOpen.Plane
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StartPlane(startPlane)
Parameters: startPlane ( NXOpen.Plane
) –New in version NX11.0.0.
License requirements: adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
SymmetricSides¶
-
JoggleBuilder.
SymmetricSides
¶ Returns or sets the symmetric sides
-------------------------------------
Getter Method
Signature
SymmetricSides()
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SymmetricSides(symmetricSides)
Parameters: symmetricSides (bool) – New in version NX11.0.0.
License requirements: adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
UseMaterialTable¶
-
JoggleBuilder.
UseMaterialTable
¶ Returns or sets the Use Material Table
-------------------------------------
Getter Method
Signature
UseMaterialTable()
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UseMaterialTable(useMaterialTable)
Parameters: useMaterialTable (bool) – New in version NX11.0.0.
License requirements: adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
Method Detail¶
CreateJoggleInputListItem¶
-
JoggleBuilder.
CreateJoggleInputListItem
¶ Create a input list item.
Signature
CreateJoggleInputListItem()
Returns: Return type: NXOpen.Features.SheetMetal.JoggleInputListItemBuilder
New in version NX11.0.0.
License requirements: adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
Validate¶
-
JoggleBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.