JoggleSideOptionsBuilder Class¶
-
class
NXOpen.Features.SheetMetal.
JoggleSideOptionsBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a Sheetmetal Joggle side Options class.
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
Clearance | Returns the clearance |
OffsetRadius | Returns the offset radius |
Runout | Returns the runout |
StationaryRadius | Returns the stationary radius |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Clearance¶
-
JoggleSideOptionsBuilder.
Clearance
¶ Returns the clearance
-------------------------------------
Getter Method
Signature
Clearance()
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
OffsetRadius¶
-
JoggleSideOptionsBuilder.
OffsetRadius
¶ Returns the offset radius
-------------------------------------
Getter Method
Signature
OffsetRadius()
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
Runout¶
-
JoggleSideOptionsBuilder.
Runout
¶ Returns the runout
-------------------------------------
Getter Method
Signature
Runout()
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
StationaryRadius¶
-
JoggleSideOptionsBuilder.
StationaryRadius
¶ Returns the stationary radius
-------------------------------------
Getter Method
Signature
StationaryRadius()
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
Method Detail¶
Validate¶
-
JoggleSideOptionsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.