FlatPatternBuilder Class¶
-
class
NXOpen.Features.SheetMetal.
FlatPatternBuilder
¶ Bases:
NXOpen.Features.SheetMetal.SheetmetalBaseBuilder
Represents a Flat Pattern feature builder.
To create a new instance of this class, use
NXOpen.Features.SheetMetal.SheetmetalManager.CreateFlatPatternBuilder()
Default values.
Property Value InnerCornerTreatment.TreatmentType None InnerCornerTreatment.UseGlobal 1 InnerCornerTreatment.Value.Value 0 (millimeters part), 0 (inches part) New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
AddedGeometry | Returns the added geometry selection |
FlatPatternViewName | Returns the flat pattern view name string |
InnerCornerTreatment | Returns the inner corner treatment corner object |
OuterCornerTreatment | Returns the outer corner treatment corner object |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
ReferenceVertex | Returns or sets the end of the edge where the tangent will define the x axis for flat as solid. |
ShowInteriorFeatureCurves | Returns or sets the show interior feature curves toggle value |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
TransformToAbsoluteCsys | Returns or sets the flag which decides if the flattened solid will be transformed to Absolute CSYS. |
UpwardFace | Returns the upward face selection |
XAxisEdge | Returns the x axis edge selection. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GenerateMoldLines | Set the flag to generate inner and outer mold lines for flat pattern features created before NX11. |
GetApplicationContext | Get the application context. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetApplicationContext | Set the application context. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AddedGeometry¶
-
FlatPatternBuilder.
AddedGeometry
¶ Returns the added geometry selection
-------------------------------------
Getter Method
Signature
AddedGeometry()
Returns: Return type: NXOpen.Section
New in version NX6.0.0.
License requirements: None.
FlatPatternViewName¶
-
FlatPatternBuilder.
FlatPatternViewName
¶ Returns the flat pattern view name string
-------------------------------------
Getter Method
Signature
FlatPatternViewName()
Returns: Return type: str New in version NX6.0.0.
License requirements: None.
InnerCornerTreatment¶
-
FlatPatternBuilder.
InnerCornerTreatment
¶ Returns the inner corner treatment corner object
-------------------------------------
Getter Method
Signature
InnerCornerTreatment()
Returns: Return type: NXOpen.Features.SheetMetal.CornerTreatmentBuilder
New in version NX6.0.0.
License requirements: None.
OuterCornerTreatment¶
-
FlatPatternBuilder.
OuterCornerTreatment
¶ Returns the outer corner treatment corner object
-------------------------------------
Getter Method
Signature
OuterCornerTreatment()
Returns: Return type: NXOpen.Features.SheetMetal.CornerTreatmentBuilder
New in version NX6.0.0.
License requirements: None.
ReferenceVertex¶
-
FlatPatternBuilder.
ReferenceVertex
¶ Returns or sets the end of the edge where the tangent will define the x axis for flat as solid.
This value will only ** be used when a face from a formed solid body is picked as Upward face. If a face from a flat solid is selected, ** this value will be ignored.
-------------------------------------
Getter Method
Signature
ReferenceVertex()
Returns: One of the end points of the reference edge. Return type: NXOpen.Point3d
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReferenceVertex(vertex)
Parameters: vertex ( NXOpen.Point3d
) – One of the end points of the reference edge.New in version NX7.5.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
ShowInteriorFeatureCurves¶
-
FlatPatternBuilder.
ShowInteriorFeatureCurves
¶ Returns or sets the show interior feature curves toggle value
-------------------------------------
Getter Method
Signature
ShowInteriorFeatureCurves()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShowInteriorFeatureCurves(showInteriorFeatureCurves)
Parameters: showInteriorFeatureCurves (bool) – New in version NX6.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
TransformToAbsoluteCsys¶
-
FlatPatternBuilder.
TransformToAbsoluteCsys
¶ Returns or sets the flag which decides if the flattened solid will be transformed to Absolute CSYS.
This flag will only be ** used if the Upward face belongs to a formed sheet metal body. If a face from a flat solid is selected, ** this value will be ignored.
-------------------------------------
Getter Method
Signature
TransformToAbsoluteCsys()
Returns: True = Transform to ABS, False = Do not transform to ABS. Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TransformToAbsoluteCsys(transformFlag)
Parameters: transformFlag (bool) – True = Transform to ABS, False = Do not transform to ABS. New in version NX7.5.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
UpwardFace¶
-
FlatPatternBuilder.
UpwardFace
¶ Returns the upward face selection
-------------------------------------
Getter Method
Signature
UpwardFace()
Returns: Return type: NXOpen.SelectFace
New in version NX6.0.0.
License requirements: None.
XAxisEdge¶
-
FlatPatternBuilder.
XAxisEdge
¶ Returns the x axis edge selection.
This edge selection is necessary when a face from a formed ** solid body is picked as Upward face. If a face from a flat solid is selected, ** this value will be ignored.
-------------------------------------
Getter Method
Signature
XAxisEdge()
Returns: Return type: NXOpen.SelectEdge
New in version NX7.5.0.
License requirements: None.
Method Detail¶
GenerateMoldLines¶
-
FlatPatternBuilder.
GenerateMoldLines
¶ Set the flag to generate inner and outer mold lines for flat pattern features created before NX11.
Signature
GenerateMoldLines()
New in version NX11.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
Validate¶
-
FlatPatternBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.