ContourFlangeBuilder Class¶
-
class
NXOpen.Features.SheetMetal.
ContourFlangeBuilder
¶ Bases:
NXOpen.Features.SheetMetal.SheetmetalBaseBuilder
Represents a Contour Flange feature builder.
To create a new instance of this class, use
NXOpen.Features.SheetMetal.SheetmetalManager.CreateContourFlangeFeatureBuilder()
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
BendOptions | Returns the bend options |
EdgeChain | Returns or sets the section having chain edges. |
IsSecondary | Returns or sets the contour flange type. |
MiterOptions | Returns the miter options |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
Section | Returns or sets the section of contour flange |
Sketch | Returns or sets the sketch |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
SweepSide | Returns or sets the projection direction of contour flange |
SweepType | Returns or sets the projection side of contour flange |
Tag | Returns the Tag for this object. |
ThicknessSide | Returns or sets the thickness side of contour flange |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetApplicationContext | Get the application context. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
GetSweepDistance | THE projection distance of contour flange @return |
GetThickness | THE thickness of contour flange @return |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetApplicationContext | Set the application context. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
SetSweepDistance | |
SetThickness | |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
ValidateBuilderData | Verify whether the builder data is valid for creating a Contour Flange or not. |
Enumerations¶
ContourFlangeBuilderSectionSideOptions Enumeration | This enum represents the side of the section in which material is created. |
ContourFlangeBuilderSweepSideOptions Enumeration | This enum represents the side in which the contour flange will be swept. |
ContourFlangeBuilderSweepTypeOptions Enumeration | This enum represents the sweep type of the contour flange |
Property Detail¶
BendOptions¶
-
ContourFlangeBuilder.
BendOptions
¶ Returns the bend options
-------------------------------------
Getter Method
Signature
BendOptions()
Returns: Return type: NXOpen.Features.SheetMetal.BendOptions
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
EdgeChain¶
-
ContourFlangeBuilder.
EdgeChain
¶ Returns or sets the section having chain edges.
-------------------------------------
Getter Method
Signature
EdgeChain()
Returns: Return type: NXOpen.Section
New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
-------------------------------------
Setter Method
Signature
EdgeChain(edgeChain)
Parameters: edgeChain ( NXOpen.Section
) –New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
IsSecondary¶
-
ContourFlangeBuilder.
IsSecondary
¶ Returns or sets the contour flange type.
-------------------------------------
Getter Method
Signature
IsSecondary()
Returns: Return type: bool New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
-------------------------------------
Setter Method
Signature
IsSecondary(isSecondary)
Parameters: isSecondary (bool) – New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
MiterOptions¶
-
ContourFlangeBuilder.
MiterOptions
¶ Returns the miter options
-------------------------------------
Getter Method
Signature
MiterOptions()
Returns: Miter data Return type: NXOpen.Features.SheetMetal.MiterOptions
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
Section¶
-
ContourFlangeBuilder.
Section
¶ Returns or sets the section of contour flange
-------------------------------------
Getter Method
Signature
Section()
Returns: section of contour flange Return type: NXOpen.Section
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
-------------------------------------
Setter Method
Signature
Section(section)
Parameters: section ( NXOpen.Section
) –New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
Sketch¶
-
ContourFlangeBuilder.
Sketch
¶ Returns or sets the sketch
-------------------------------------
Getter Method
Signature
Sketch()
Returns: sketch Return type: NXOpen.Features.SketchFeature
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
-------------------------------------
Setter Method
Signature
Sketch(sketch)
Parameters: sketch ( NXOpen.Features.SketchFeature
) – sketchNew in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
SweepSide¶
-
ContourFlangeBuilder.
SweepSide
¶ Returns or sets the projection direction of contour flange
-------------------------------------
Getter Method
Signature
SweepSide()
Returns: Return type: NXOpen.Features.SheetMetal.ContourFlangeBuilderSweepSideOptions
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
-------------------------------------
Setter Method
Signature
SweepSide(sweepSide)
Parameters: sweepSide ( NXOpen.Features.SheetMetal.ContourFlangeBuilderSweepSideOptions
) –New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
SweepType¶
-
ContourFlangeBuilder.
SweepType
¶ Returns or sets the projection side of contour flange
-------------------------------------
Getter Method
Signature
SweepType()
Returns: Return type: NXOpen.Features.SheetMetal.ContourFlangeBuilderSweepTypeOptions
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
-------------------------------------
Setter Method
Signature
SweepType(sweepType)
Parameters: sweepType ( NXOpen.Features.SheetMetal.ContourFlangeBuilderSweepTypeOptions
) –New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
ThicknessSide¶
-
ContourFlangeBuilder.
ThicknessSide
¶ Returns or sets the thickness side of contour flange
-------------------------------------
Getter Method
Signature
ThicknessSide()
Returns: Return type: NXOpen.Features.SheetMetal.ContourFlangeBuilderSectionSideOptions
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
-------------------------------------
Setter Method
Signature
ThicknessSide(sectionSide)
Parameters: sectionSide ( NXOpen.Features.SheetMetal.ContourFlangeBuilderSectionSideOptions
) –New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
Method Detail¶
GetSweepDistance¶
-
ContourFlangeBuilder.
GetSweepDistance
¶ THE projection distance of contour flange
Signature
GetSweepDistance()
Returns: Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
GetThickness¶
-
ContourFlangeBuilder.
GetThickness
¶ THE thickness of contour flange
Signature
GetThickness()
Returns: Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
SetSweepDistance¶
-
ContourFlangeBuilder.
SetSweepDistance
¶ Signature
SetSweepDistance(sweepDistance)
Parameters: sweepDistance (str) – New in version NX4.0.0.
Deprecated since version NX10.0.0: Use
Expression.RightHandSide()
on theExpression
object returned fromFeatures.SheetMetal.ContourFlangeBuilder.GetSweepDistance()
instead.License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
SetThickness¶
-
ContourFlangeBuilder.
SetThickness
¶ Signature
SetThickness(thickness)
Parameters: thickness (str) – New in version NX4.0.0.
Deprecated since version NX10.0.0: Use
Expression.RightHandSide()
on theExpression
object returned fromFeatures.SheetMetal.ContourFlangeBuilder.GetThickness()
instead.License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
Validate¶
-
ContourFlangeBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.
ValidateBuilderData¶
-
ContourFlangeBuilder.
ValidateBuilderData
¶ Verify whether the builder data is valid for creating a Contour Flange or not.
If the Builder data is valid, returned value shall be 0
Signature
ValidateBuilderData()
Returns: Data Validity Flag. Return type: int New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)