ClosedCornerBuilder Class¶
-
class
NXOpen.Features.SheetMetal.
ClosedCornerBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a Closed corner feature builder.
To create a new instance of this class, use
NXOpen.Features.SheetMetal.SheetmetalManager.CreateClosedCornerFeatureBuilder()
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
BlendMiter | Returns or sets the option for smooth transition from miter to cutout edges. |
ClosureType | Returns or sets the closure type |
Diameter | Returns the diameter. |
Gap | Returns the gap. |
MiterCorner | Returns or sets the corner will be closed using the miter algorithm. |
Offset | Returns the value by which relief origin will be offset |
Origin | Returns or sets the default origin will be at the corner point instead of the intersection of bend centerlines. |
Overlap | Returns the overlap. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
RectangularLength | Returns the length of rectangular relief. |
RectangularWidth | Returns the width of rectangular relief. |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
TreatmentType | Returns or sets the treatment type |
Type | Returns or sets the feature type |
VAngle1 | Returns the angle1 of V relief. |
VAngle2 | Returns the angle2 of V relief. |
Methods¶
Method | Description |
---|---|
AddFacePair | Add a face pair. |
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFacePair | Return the face pair. |
GetFeature | Returns the feature currently being edited by this builder. |
GetNumberOfFacePairs | Returns the number of face pairs already identified for the three bend corner feature. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
RemoveFacePair | Removes a face pair (that represents a unique corner) from the list of face pairs already added. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
ValidateBuilderData | Validates the builder data. |
Enumerations¶
ClosedCornerBuilderClosureTypeOptions Enumeration | This enum represents Corner Closure type |
ClosedCornerBuilderOriginTypes Enumeration | This enum represents Origin type |
ClosedCornerBuilderTreatmentTypeOptions Enumeration | This enum represents Corner treatment type |
ClosedCornerBuilderTypes Enumeration | This enum represents the feature types. |
Property Detail¶
BlendMiter¶
-
ClosedCornerBuilder.
BlendMiter
¶ Returns or sets the option for smooth transition from miter to cutout edges.
-------------------------------------
Getter Method
Signature
BlendMiter()
Returns: Return type: bool New in version NX8.5.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
-------------------------------------
Setter Method
Signature
BlendMiter(blendMiter)
Parameters: blendMiter (bool) – New in version NX8.5.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
ClosureType¶
-
ClosedCornerBuilder.
ClosureType
¶ Returns or sets the closure type
-------------------------------------
Getter Method
Signature
ClosureType()
Returns: The type of closure specified for the corner Return type: NXOpen.Features.SheetMetal.ClosedCornerBuilderClosureTypeOptions
New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
-------------------------------------
Setter Method
Signature
ClosureType(closureType)
Parameters: closureType ( NXOpen.Features.SheetMetal.ClosedCornerBuilderClosureTypeOptions
) – The type of closure specified for the cornerNew in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
Diameter¶
-
ClosedCornerBuilder.
Diameter
¶ Returns the diameter.
-------------------------------------
Getter Method
Signature
Diameter()
Returns: The diameter for relief Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
Gap¶
-
ClosedCornerBuilder.
Gap
¶ Returns the gap.
-------------------------------------
Getter Method
Signature
Gap()
Returns: The gap. Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
MiterCorner¶
-
ClosedCornerBuilder.
MiterCorner
¶ Returns or sets the corner will be closed using the miter algorithm.
-------------------------------------
Getter Method
Signature
MiterCorner()
Returns: Return type: bool New in version NX7.5.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
-------------------------------------
Setter Method
Signature
MiterCorner(miterCorner)
Parameters: miterCorner (bool) – New in version NX7.5.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
Offset¶
-
ClosedCornerBuilder.
Offset
¶ Returns the value by which relief origin will be offset
-------------------------------------
Getter Method
Signature
Offset()
Returns: The Offset Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
Origin¶
-
ClosedCornerBuilder.
Origin
¶ Returns or sets the default origin will be at the corner point instead of the intersection of bend centerlines.
-------------------------------------
Getter Method
Signature
Origin()
Returns: The default location of relief origin Return type: NXOpen.Features.SheetMetal.ClosedCornerBuilderOriginTypes
New in version NX6.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
-------------------------------------
Setter Method
Signature
Origin(originType)
Parameters: originType ( NXOpen.Features.SheetMetal.ClosedCornerBuilderOriginTypes
) – The default location of relief originNew in version NX6.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
Overlap¶
-
ClosedCornerBuilder.
Overlap
¶ Returns the overlap.
-------------------------------------
Getter Method
Signature
Overlap()
Returns: The overlap Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
RectangularLength¶
-
ClosedCornerBuilder.
RectangularLength
¶ Returns the length of rectangular relief.
The length is associated to the first bend selected.
-------------------------------------
Getter Method
Signature
RectangularLength()
Returns: The Length Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
RectangularWidth¶
-
ClosedCornerBuilder.
RectangularWidth
¶ Returns the width of rectangular relief.
The width is associated to the second bend selected.
-------------------------------------
Getter Method
Signature
RectangularWidth()
Returns: The Width Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
TreatmentType¶
-
ClosedCornerBuilder.
TreatmentType
¶ Returns or sets the treatment type
-------------------------------------
Getter Method
Signature
TreatmentType()
Returns: The type of treatment specified for the corner Return type: NXOpen.Features.SheetMetal.ClosedCornerBuilderTreatmentTypeOptions
New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
-------------------------------------
Setter Method
Signature
TreatmentType(treatmentType)
Parameters: treatmentType ( NXOpen.Features.SheetMetal.ClosedCornerBuilderTreatmentTypeOptions
) – The type of treatment specified for the cornerNew in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
Type¶
-
ClosedCornerBuilder.
Type
¶ Returns or sets the feature type
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.Features.SheetMetal.ClosedCornerBuilderTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(type)
Parameters: type ( NXOpen.Features.SheetMetal.ClosedCornerBuilderTypes
) –New in version NX6.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
VAngle1¶
-
ClosedCornerBuilder.
VAngle1
¶ Returns the angle1 of V relief.
This is the angle associated with the first bend selected.
-------------------------------------
Getter Method
Signature
VAngle1()
Returns: The Angle1 Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
VAngle2¶
-
ClosedCornerBuilder.
VAngle2
¶ Returns the angle2 of V relief.
This is the angle associated to the second bend selected.
-------------------------------------
Getter Method
Signature
VAngle2()
Returns: The Angle2 Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
Method Detail¶
AddFacePair¶
-
ClosedCornerBuilder.
AddFacePair
¶ Add a face pair.
Signature
AddFacePair(firstFace, secondFace)
Parameters: - firstFace (
NXOpen.Face
) – A bend face from a bend - secondFace (
NXOpen.Face
) – A bend face from an adjacent bend
New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
- firstFace (
GetFacePair¶
-
ClosedCornerBuilder.
GetFacePair
¶ Return the face pair.
Signature
GetFacePair(index)
Parameters: index (int) – Index of the desired face pair Returns: a tuple Return type: A tuple consisting of (firstFace, secondFace). firstFace is a NXOpen.Face
. First face of the face pair secondFace is aNXOpen.Face
. Second face of the face pairNew in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
GetNumberOfFacePairs¶
-
ClosedCornerBuilder.
GetNumberOfFacePairs
¶ Returns the number of face pairs already identified for the three bend corner feature.
Signature
GetNumberOfFacePairs()
Returns: The number of face pairs currently identified Return type: int New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
RemoveFacePair¶
-
ClosedCornerBuilder.
RemoveFacePair
¶ Removes a face pair (that represents a unique corner) from the list of face pairs already added.
Signature
RemoveFacePair(firstFace, secondFace)
Parameters: - firstFace (
NXOpen.Face
) – A face from an already selected face pair - secondFace (
NXOpen.Face
) – The other face from the face pair
New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
- firstFace (
Validate¶
-
ClosedCornerBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.