ClosedCornerBuilderTreatmentTypeOptions Enumeration¶
NXOpen.Features.SheetMetal.ClosedCornerBuilder.TreatmentTypeOptions is an alias for NXOpen.Features.SheetMetal.ClosedCornerBuilderTreatmentTypeOptions
-
class
NXOpen.Features.SheetMetal.
ClosedCornerBuilderTreatmentTypeOptions
¶ Bases:
object
This enum represents Corner treatment type
Enum Members
Enum Member Enum Member Description Open Only Webs will be closedClosed Bend and Webs will be closedCircularCutout Circular shaped reliefUCutout U shaped reliefVCutout V shaped reliefRectangularCutout Rectangular shaped relief-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-