BeadBuilder Class¶
-
class
NXOpen.Features.SheetMetal.
BeadBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a Bead feature builder.
To create a new instance of this class, use
NXOpen.Features.SheetMetal.SheetmetalManager.CreateBeadFeatureBuilder()
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
Angle | Returns the angle of the bead. |
CrossSectionType | Returns or sets the bead profile type . |
DieRadius | Returns the bead die radius. |
EndType | Returns or sets the bead end type . |
Height | Returns the height of the bead. |
HeightSide | Returns or sets the Height side for the bead. |
IncludeRounding | Returns or sets the rounding type . |
MinimumToolClearance | Returns the Minimum tool clearance expression. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
PunchRadius | Returns the bead punch radius. |
PunchedWidth | Returns the Punched width of the bead. |
Radius | Returns the radius of the bead. |
Section | Returns or sets the Section used by the bead. |
Sketch | Returns or sets the Slave Sketch used by the Bead, If one exists. |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
TaperDistance | Returns the taper distance of the bead. |
Width | Returns the width of the bead. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetAngle | |
SetDieRadius | |
SetHeight | |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
SetPunchRadius | |
SetPunchedWidth | |
SetRadius | |
SetWidth | |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
ValidateBuilderData | Verify whether the builder data is valid for creating a Bead or not. |
Enumerations¶
BeadBuilderCrossSectionTypeOptions Enumeration | This enum represents the cross section type options for the Bead. |
BeadBuilderEndTypeOptions Enumeration | This enum represents the end type options for the Bead. |
BeadBuilderHeightSideOptions Enumeration | This enum represents the depth direction for the Bead. |
Property Detail¶
Angle¶
-
BeadBuilder.
Angle
¶ Returns the angle of the bead.
-------------------------------------
Getter Method
Signature
Angle()
Returns: Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
CrossSectionType¶
-
BeadBuilder.
CrossSectionType
¶ Returns or sets the bead profile type .
Specify
NXOpen.Features.SheetMetal.BeadBuilderCrossSectionTypeOptions.Circular
to have profile of half circle. SpecifyNXOpen.Features.SheetMetal.BeadBuilderCrossSectionTypeOptions.Ushaped
to have profile of U shape. SpecifyNXOpen.Features.SheetMetal.BeadBuilderCrossSectionTypeOptions.Vshaped
to have profile of V shape.-------------------------------------
Getter Method
Signature
CrossSectionType()
Returns: Return type: NXOpen.Features.SheetMetal.BeadBuilderCrossSectionTypeOptions
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
-------------------------------------
Setter Method
Signature
CrossSectionType(crossSectionOption)
Parameters: crossSectionOption ( NXOpen.Features.SheetMetal.BeadBuilderCrossSectionTypeOptions
) –New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
DieRadius¶
-
BeadBuilder.
DieRadius
¶ Returns the bead die radius.
-------------------------------------
Getter Method
Signature
DieRadius()
Returns: Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
EndType¶
-
BeadBuilder.
EndType
¶ Returns or sets the bead end type .
Specify
NXOpen.Features.SheetMetal.BeadBuilderEndTypeOptions.Formed
to have ends of bead feature be formed. SpecifyNXOpen.Features.SheetMetal.BeadBuilderEndTypeOptions.Lanced
to have ends of bead feature be Lanced. SpecifyNXOpen.Features.SheetMetal.BeadBuilderEndTypeOptions.Punched
to have ends of bead feature be Punched. SpecifyNXOpen.Features.SheetMetal.BeadBuilderEndTypeOptions.Tapered
to have ends of bead feature be Tapered.-------------------------------------
Getter Method
Signature
EndType()
Returns: Return type: NXOpen.Features.SheetMetal.BeadBuilderEndTypeOptions
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
-------------------------------------
Setter Method
Signature
EndType(beadEndOptions)
Parameters: beadEndOptions ( NXOpen.Features.SheetMetal.BeadBuilderEndTypeOptions
) –New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
Height¶
-
BeadBuilder.
Height
¶ Returns the height of the bead.
-------------------------------------
Getter Method
Signature
Height()
Returns: Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
HeightSide¶
-
BeadBuilder.
HeightSide
¶ Returns or sets the Height side for the bead.
This is used to specify the direction in which the Bead is created. If Bead creation must happen in the direction of the Section Normal (specified using the
NXOpen.Features.SheetMetal.BeadBuilder.Section`()
) then pass the value ofNXOpen.Features.SheetMetal.BeadBuilderHeightSideOptions.SectionNormalSide
If Bead creation must happen in the opposite direction to that of Section Normal, set the value to beNXOpen.Features.SheetMetal.BeadBuilderHeightSideOptions.SectionReverseNormalSide
-------------------------------------
Getter Method
Signature
HeightSide()
Returns: Return type: NXOpen.Features.SheetMetal.BeadBuilderHeightSideOptions
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
-------------------------------------
Setter Method
Signature
HeightSide(heightSide)
Parameters: heightSide ( NXOpen.Features.SheetMetal.BeadBuilderHeightSideOptions
) –New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
IncludeRounding¶
-
BeadBuilder.
IncludeRounding
¶ Returns or sets the rounding type .
Specify true to Round the Sharp edges. Specify false to avoid rounding.
-------------------------------------
Getter Method
Signature
IncludeRounding()
Returns: Return type: bool New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
-------------------------------------
Setter Method
Signature
IncludeRounding(rounding)
Parameters: rounding (bool) – New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
MinimumToolClearance¶
-
BeadBuilder.
MinimumToolClearance
¶ Returns the Minimum tool clearance expression.
-------------------------------------
Getter Method
Signature
MinimumToolClearance()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
PunchRadius¶
-
BeadBuilder.
PunchRadius
¶ Returns the bead punch radius.
-------------------------------------
Getter Method
Signature
PunchRadius()
Returns: Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
PunchedWidth¶
-
BeadBuilder.
PunchedWidth
¶ Returns the Punched width of the bead.
-------------------------------------
Getter Method
Signature
PunchedWidth()
Returns: Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
Radius¶
-
BeadBuilder.
Radius
¶ Returns the radius of the bead.
-------------------------------------
Getter Method
Signature
Radius()
Returns: Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
Section¶
-
BeadBuilder.
Section
¶ Returns or sets the Section used by the bead.
section should be open.
-------------------------------------
Getter Method
Signature
Section()
Returns: Return type: NXOpen.Section
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
-------------------------------------
Setter Method
Signature
Section(section)
Parameters: section ( NXOpen.Section
) –New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
Sketch¶
-
BeadBuilder.
Sketch
¶ Returns or sets the Slave Sketch used by the Bead, If one exists.
If the Sketch is created internally as part of the Bead command in the UI, then it shall be consumed by the Bead and shall not show up as a separate feature in the Part Navigator. If such a behaviour is deired, then specify the Sketch here.
-------------------------------------
Getter Method
Signature
Sketch()
Returns: Return type: NXOpen.Features.SketchFeature
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
-------------------------------------
Setter Method
Signature
Sketch(sketch)
Parameters: sketch ( NXOpen.Features.SketchFeature
) –New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
TaperDistance¶
-
BeadBuilder.
TaperDistance
¶ Returns the taper distance of the bead.
-------------------------------------
Getter Method
Signature
TaperDistance()
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
Width¶
-
BeadBuilder.
Width
¶ Returns the width of the bead.
-------------------------------------
Getter Method
Signature
Width()
Returns: Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
Method Detail¶
SetAngle¶
-
BeadBuilder.
SetAngle
¶ Signature
SetAngle(beadAngle)
Parameters: beadAngle (str) – New in version NX4.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.Expression.RightHandSide()
on theNXOpen.Expression
object returned fromNXOpen.Features.SheetMetal.BeadBuilder.Angle()
instead.License requirements: nx_sheet_metal (“NX Sheet Metal”)
SetDieRadius¶
-
BeadBuilder.
SetDieRadius
¶ Signature
SetDieRadius(beadDieRadius)
Parameters: beadDieRadius (str) – New in version NX4.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.Expression.RightHandSide()
on theNXOpen.Expression
object returned fromNXOpen.Features.SheetMetal.BeadBuilder.DieRadius()
instead.License requirements: nx_sheet_metal (“NX Sheet Metal”)
SetHeight¶
-
BeadBuilder.
SetHeight
¶ Signature
SetHeight(beadHeight)
Parameters: beadHeight (str) – New in version NX4.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.Expression.RightHandSide()
on theNXOpen.Expression
object returned fromNXOpen.Features.SheetMetal.BeadBuilder.Height()
instead.License requirements: nx_sheet_metal (“NX Sheet Metal”)
SetPunchRadius¶
-
BeadBuilder.
SetPunchRadius
¶ Signature
SetPunchRadius(punchRadius)
Parameters: punchRadius (str) – New in version NX4.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.Expression.RightHandSide()
on theNXOpen.Expression
object returned fromNXOpen.Features.SheetMetal.BeadBuilder.PunchRadius()
instead.License requirements: nx_sheet_metal (“NX Sheet Metal”)
SetPunchedWidth¶
-
BeadBuilder.
SetPunchedWidth
¶ Signature
SetPunchedWidth(punchedWidth)
Parameters: punchedWidth (str) – New in version NX4.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.Expression.RightHandSide()
on theNXOpen.Expression
object returned fromNXOpen.Features.SheetMetal.BeadBuilder.PunchedWidth()
instead.License requirements: nx_sheet_metal (“NX Sheet Metal”)
SetRadius¶
-
BeadBuilder.
SetRadius
¶ Signature
SetRadius(beadRadius)
Parameters: beadRadius (str) – New in version NX4.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.Expression.RightHandSide()
on theNXOpen.Expression
object returned fromNXOpen.Features.SheetMetal.BeadBuilder.Radius()
instead.License requirements: nx_sheet_metal (“NX Sheet Metal”)
SetWidth¶
-
BeadBuilder.
SetWidth
¶ Signature
SetWidth(beadWidth)
Parameters: beadWidth (str) – New in version NX4.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.Expression.RightHandSide()
on theNXOpen.Expression
object returned fromNXOpen.Features.SheetMetal.BeadBuilder.Width()
instead.License requirements: nx_sheet_metal (“NX Sheet Metal”)
Validate¶
-
BeadBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.
ValidateBuilderData¶
-
BeadBuilder.
ValidateBuilderData
¶ Verify whether the builder data is valid for creating a Bead or not.
If the Builder data is valid, returned value shall be 0
Signature
ValidateBuilderData()
Returns: Data Validity Flag. Return type: int New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)