SewBuilder Class¶
-
class
NXOpen.Features.
SewBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.Sew
builder.Inputs to this class can be convergent objects.
To create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateSewBuilder()
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
IsCommonFacesSearched | Returns or sets the common faces. |
OutputMultipleSheets | Returns or sets the output multiple sheets |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
SewAllInstances | Returns or sets the sew all instances |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
TargetBodies | Returns the target sheet bodies |
TargetFaces | Returns the target solid faces |
Tolerance | Returns or sets the tolerance |
ToolBodies | Returns the tool sheet bodies |
ToolFaces | Returns the tool solid faces |
Type | Returns or sets the sew type |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
GetUnsewnBodies | The unsewn bodies @return the input objects not sewn into this feature |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
SewBuilderTypes Enumeration | Specifies the sew type. |
Property Detail¶
IsCommonFacesSearched¶
-
SewBuilder.
IsCommonFacesSearched
¶ Returns or sets the common faces.
If true, the common faces are searched when the sew type is solid
-------------------------------------
Getter Method
Signature
IsCommonFacesSearched()
Returns: Return type: bool New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
-------------------------------------
Setter Method
Signature
IsCommonFacesSearched(isCommonFacesSearched)
Parameters: isCommonFacesSearched (bool) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
OutputMultipleSheets¶
-
SewBuilder.
OutputMultipleSheets
¶ Returns or sets the output multiple sheets
-------------------------------------
Getter Method
Signature
OutputMultipleSheets()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OutputMultipleSheets(outputMultipleSheets)
Parameters: outputMultipleSheets (bool) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
SewAllInstances¶
-
SewBuilder.
SewAllInstances
¶ Returns or sets the sew all instances
-------------------------------------
Getter Method
Signature
SewAllInstances()
Returns: Return type: bool New in version NX5.0.0.
Deprecated since version NX9.0.0: This is for pre NX8 usage; new features cannot be created by using this option in NX8 or later, it is safe to remove this call for post-NX8.
License requirements: None.
-------------------------------------
Setter Method
Signature
SewAllInstances(sewAllInstances)
Parameters: sewAllInstances (bool) – New in version NX5.0.0.
Deprecated since version NX9.0.0: This is for pre NX8 usage; new features cannot be created by using this option in NX8 or later, it is safe to remove this call for post-NX8.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
TargetBodies¶
-
SewBuilder.
TargetBodies
¶ Returns the target sheet bodies
-------------------------------------
Getter Method
Signature
TargetBodies()
Returns: Return type: NXOpen.SelectDisplayableObjectList
New in version NX5.0.0.
License requirements: None.
TargetFaces¶
-
SewBuilder.
TargetFaces
¶ Returns the target solid faces
-------------------------------------
Getter Method
Signature
TargetFaces()
Returns: Return type: NXOpen.SelectFaceList
New in version NX5.0.0.
License requirements: None.
Tolerance¶
-
SewBuilder.
Tolerance
¶ Returns or sets the tolerance
-------------------------------------
Getter Method
Signature
Tolerance()
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Tolerance(tolerance)
Parameters: tolerance (float) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
ToolBodies¶
-
SewBuilder.
ToolBodies
¶ Returns the tool sheet bodies
-------------------------------------
Getter Method
Signature
ToolBodies()
Returns: Return type: NXOpen.SelectDisplayableObjectList
New in version NX5.0.0.
License requirements: None.
ToolFaces¶
-
SewBuilder.
ToolFaces
¶ Returns the tool solid faces
-------------------------------------
Getter Method
Signature
ToolFaces()
Returns: Return type: NXOpen.SelectFaceList
New in version NX5.0.0.
License requirements: None.
Type¶
-
SewBuilder.
Type
¶ Returns or sets the sew type
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.Features.SewBuilderTypes
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(type)
Parameters: type ( NXOpen.Features.SewBuilderTypes
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
Method Detail¶
GetUnsewnBodies¶
-
SewBuilder.
GetUnsewnBodies
¶ The unsewn bodies
Signature
GetUnsewnBodies()
Returns: the input objects not sewn into this feature Return type: list of NXOpen.NXObject
New in version NX8.0.0.
License requirements: None.
Validate¶
-
SewBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.