SewBuilderTypes Enumeration

NXOpen.Features.SewBuilder.Types is an alias for NXOpen.Features.SewBuilderTypes

class NXOpen.Features.SewBuilderTypes

Bases: object

Specifies the sew type.

Enum Members

Enum Member Enum Member Description
Sheet
Sheet
Solid
Solid
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.