ResizeFaceBuilder Class¶
-
class
NXOpen.Features.
ResizeFaceBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a builder for a resize face feature, don’t use it until nx502.
To create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateResizeFaceBuilder()
New in version NX5.0.2.
Properties¶
Property | Description |
---|---|
Angle | Returns the angle to resize, only for cones. |
BlendFace | Returns the face collector holding the all the recognized blend faces adjacent to faces to resize. |
Diameter | Returns the diameter to resize, only for cylinderical and sphere faces, don’t use it until nx502 |
Face | Returns the faces to resize, don’t use it until nx502 |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Angle¶
-
ResizeFaceBuilder.
Angle
¶ Returns the angle to resize, only for cones.
don’t use it until nx502
-------------------------------------
Getter Method
Signature
Angle()
Returns: the angle expression Return type: NXOpen.Expression
New in version NX5.0.2.
License requirements: None.
BlendFace¶
-
ResizeFaceBuilder.
BlendFace
¶ Returns the face collector holding the all the recognized blend faces adjacent to faces to resize.
It is auto recognized blends + user selected blends - user excluded blends, don’t use it until nx502
-------------------------------------
Getter Method
Signature
BlendFace()
Returns: the adjacent blends builder Return type: NXOpen.ModlDirect.SelectBlend
New in version NX5.0.2.
License requirements: None.
Diameter¶
-
ResizeFaceBuilder.
Diameter
¶ Returns the diameter to resize, only for cylinderical and sphere faces, don’t use it until nx502
-------------------------------------
Getter Method
Signature
Diameter()
Returns: the diameter expression Return type: NXOpen.Expression
New in version NX5.0.2.
License requirements: None.
Face¶
-
ResizeFaceBuilder.
Face
¶ Returns the faces to resize, don’t use it until nx502
-------------------------------------
Getter Method
Signature
Face()
Returns: the faces to resize, only support cylindrical, sphere and cone faces Return type: NXOpen.SelectFaceList
New in version NX5.0.2.
License requirements: None.
Method Detail¶
Validate¶
-
ResizeFaceBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.