PatternFaceFeatureBuilder Class¶
-
class
NXOpen.Features.
PatternFaceFeatureBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a builder for a pattern face feature, post NX9.
To create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreatePatternFaceFeatureBuilder()
Default values.
Property Value CopyChamferLabels false PatternDefinition.AlongPathDefinition.XOnPathSpacing.NCopies.Value 2 PatternDefinition.AlongPathDefinition.XOnPathSpacing.SpaceType Offset PatternDefinition.AlongPathDefinition.XPathOption Offset PatternDefinition.AlongPathDefinition.YDirectionOption Section PatternDefinition.AlongPathDefinition.YOnPathSpacing.NCopies.Value 1 PatternDefinition.AlongPathDefinition.YPathOption Offset PatternDefinition.AlongPathDefinition.YSpacing.NCopies.Value 1 PatternDefinition.AlongPathDefinition.YSpacing.PitchDistance.Value 10 (millimeters part), 1 (inches part) PatternDefinition.AlongPathDefinition.YSpacing.SpaceType Offset PatternDefinition.AlongPathDefinition.YSpacing.SpanDistance.Value 100 (millimeters part), 10 (inches part) PatternDefinition.CircularDefinition.AngularSpacing.NCopies.Value 12 PatternDefinition.CircularDefinition.AngularSpacing.PitchAngle.Value 30 PatternDefinition.CircularDefinition.AngularSpacing.PitchDistance.Value 10 (millimeters part), 1 (inches part) PatternDefinition.CircularDefinition.AngularSpacing.SpaceType Offset PatternDefinition.CircularDefinition.AngularSpacing.SpanAngle.Value 360 (millimeters part), 360 (inches part) PatternDefinition.CircularDefinition.AngularSpacing.UsePitchOption Angle PatternDefinition.CircularDefinition.CreateLastStaggered true PatternDefinition.CircularDefinition.HorizontalRef.RotationAngle.Value 0 (millimeters part), 0 (inches part) PatternDefinition.CircularDefinition.IncludeSeedToggle true PatternDefinition.CircularDefinition.RadialSpacing.NCopies.Value 1 PatternDefinition.CircularDefinition.StaggerType None PatternDefinition.HelixDefinition.AnglePitch.Value 30 PatternDefinition.HelixDefinition.CountOfInstances.Value 6 PatternDefinition.HelixDefinition.DirectionType Righthand PatternDefinition.HelixDefinition.DistancePitch.Value 10 (millimeters part), 0.4 (inches part) PatternDefinition.HelixDefinition.HelixPitch.Value 50 (millimeters part), 2 (inches part) PatternDefinition.HelixDefinition.HelixSpan.Value 100 (millimeters part), 4 (inches part) PatternDefinition.HelixDefinition.NumberOfTurns.Value 2 PatternDefinition.HelixDefinition.SizeOption CountAngleDistance PatternDefinition.PatternFill.FillMargin.Value 0 (millimeters part), 0 (inches part) PatternDefinition.PatternFill.FillOptions None PatternDefinition.PatternFill.SimplifiedBoundaryToggle False PatternDefinition.PatternOrientation.AlongOrientationOption NormalToPath PatternDefinition.PatternOrientation.CircularOrientationOption FollowPattern PatternDefinition.PatternOrientation.FollowFaceProjDirOption PatternPlaneNormal PatternDefinition.PatternOrientation.GeneralOrientationOption Fixed PatternDefinition.PatternOrientation.HelixOrientationOption FollowPattern PatternDefinition.PatternOrientation.LinearOrientationOption Fixed PatternDefinition.PatternOrientation.MirrorOrientationOption FollowPattern PatternDefinition.PatternOrientation.OrientationOption Fixed PatternDefinition.PatternOrientation.PolygonOrientationOption FollowPattern PatternDefinition.PatternOrientation.SpiralOrientationOption FollowPattern PatternDefinition.PatternType Linear PatternDefinition.PolygonDefinition.NumberOfSides.Value 6 PatternDefinition.PolygonDefinition.PolygonSizeOption Inscribed PatternDefinition.PolygonDefinition.PolygonSpacing.NCopies.Value 4 PatternDefinition.PolygonDefinition.PolygonSpacing.PitchDistance.Value 25 (millimeters part), 1 (inches part) PatternDefinition.PolygonDefinition.PolygonSpacing.SpaceType Offset PatternDefinition.PolygonDefinition.PolygonSpacing.SpanAngle.Value 360 PatternDefinition.PolygonDefinition.RadialSpacing.NCopies.Value 1 PatternDefinition.PolygonDefinition.RadialSpacing.PitchDistance.Value 25 (millimeters part), 1 (inches part) PatternDefinition.PolygonDefinition.RadialSpacing.SpanDistance.Value 100 (millimeters part), 4 (inches part) PatternDefinition.RectangularDefinition.CreateLastStaggered true PatternDefinition.RectangularDefinition.SimplifiedLayoutType Square PatternDefinition.RectangularDefinition.StaggerType None PatternDefinition.RectangularDefinition.XSpacing.NCopies.Value 2 PatternDefinition.RectangularDefinition.YSpacing.NCopies.Value 1 PatternDefinition.SpiralDefinition.DirectionType Lefthand PatternDefinition.SpiralDefinition.NumberOfTurns.Value 1 (millimeters part), 1 (inches part) PatternDefinition.SpiralDefinition.RadialPitch.Value 50 (millimeters part), 2 (inches part) PatternDefinition.SpiralDefinition.SizeSpiralType NumberOfTurns PatternDefinition.SpiralDefinition.TotalAngle.Value 360 (millimeters part), 360 (inches part) New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
CopyChamferLabels | Returns or sets the chamfer label options . |
FaceCollector | Returns the face collector. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
PatternDefinition | Returns the pattern definition service. |
ReferencePoint | Returns the reference point service. |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
CopyChamferLabels¶
-
PatternFaceFeatureBuilder.
CopyChamferLabels
¶ Returns or sets the chamfer label options .
‘true’ if the chamfer faces should be labeled automatically ‘false’ if the chamfer faces should not be labeled automatically
-------------------------------------
Getter Method
Signature
CopyChamferLabels()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CopyChamferLabels(shouldLabelChamfer)
Parameters: shouldLabelChamfer (bool) – New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
FaceCollector¶
-
PatternFaceFeatureBuilder.
FaceCollector
¶ Returns the face collector.
Collects the input faces to pattern
-------------------------------------
Getter Method
Signature
FaceCollector()
Returns: Return type: NXOpen.ScCollector
New in version NX9.0.0.
License requirements: None.
PatternDefinition¶
-
PatternFaceFeatureBuilder.
PatternDefinition
¶ Returns the pattern definition service.
This is the object that determines the type of pattern and holds the associated data that comes with it.
-------------------------------------
Getter Method
Signature
PatternDefinition()
Returns: Return type: NXOpen.GeometricUtilities.PatternDefinition
New in version NX9.0.0.
License requirements: None.
ReferencePoint¶
-
PatternFaceFeatureBuilder.
ReferencePoint
¶ Returns the reference point service.
This contains the origin for creating pattern based transformations
-------------------------------------
Getter Method
Signature
ReferencePoint()
Returns: Return type: NXOpen.GeometricUtilities.PatternReferencePointServiceBuilder
New in version NX9.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
PatternFaceFeatureBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.