HelixBuilder Class¶
-
class
NXOpen.Features.
HelixBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.Helix
builderTo create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateHelixBuilder()
Default values.
Property Value LengthMethod Limits PitchLaw.Function ft PitchLaw.LawType Constant PitchLaw.Parameter t SizeOption Diameter TurnDirection RightHand Type AlongVector New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
AngleTolerance | Returns or sets the angle tolerance |
CoordinateSystem | Returns or sets the coordinate system |
DistanceTolerance | Returns or sets the distance tolerance |
EndLimit | Returns the end limit |
LengthMethod | Returns or sets the length method |
NumberOfTurns | Returns or sets the number of turns |
OrientationOption | Returns or sets the orientation option |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
PitchLaw | Returns the pitch |
SizeLaw | Returns the size law |
SizeOption | Returns or sets the size option |
Spine | Returns the length spine |
StartAngle | Returns the start angle |
StartLimit | Returns the start limit |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
TurnDirection | Returns or sets the turn direction |
Type | Returns or sets the type |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
Evaluate | Evaluates the curve |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
HelixBuilderLengthMethods Enumeration | Method for defining the length |
HelixBuilderOrientationOptions Enumeration | Orientation options for along spine type |
HelixBuilderSizeOptions Enumeration | Option indicating how size is defined |
HelixBuilderTurnDirections Enumeration | Option indicating direction of the turn |
HelixBuilderTypes Enumeration | Type of helix |
Property Detail¶
AngleTolerance¶
-
HelixBuilder.
AngleTolerance
¶ Returns or sets the angle tolerance
-------------------------------------
Getter Method
Signature
AngleTolerance()
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AngleTolerance(angleTolerance)
Parameters: angleTolerance (float) – New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
CoordinateSystem¶
-
HelixBuilder.
CoordinateSystem
¶ Returns or sets the coordinate system
-------------------------------------
Getter Method
Signature
CoordinateSystem()
Returns: Return type: NXOpen.CoordinateSystem
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CoordinateSystem(coordinateSystem)
Parameters: coordinateSystem ( NXOpen.CoordinateSystem
) –New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
DistanceTolerance¶
-
HelixBuilder.
DistanceTolerance
¶ Returns or sets the distance tolerance
-------------------------------------
Getter Method
Signature
DistanceTolerance()
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DistanceTolerance(distanceTolerance)
Parameters: distanceTolerance (float) – New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
EndLimit¶
-
HelixBuilder.
EndLimit
¶ Returns the end limit
-------------------------------------
Getter Method
Signature
EndLimit()
Returns: Return type: NXOpen.GeometricUtilities.OnPathDimensionBuilder
New in version NX8.5.0.
License requirements: None.
LengthMethod¶
-
HelixBuilder.
LengthMethod
¶ Returns or sets the length method
-------------------------------------
Getter Method
Signature
LengthMethod()
Returns: Return type: NXOpen.Features.HelixBuilderLengthMethods
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LengthMethod(lengthMethod)
Parameters: lengthMethod ( NXOpen.Features.HelixBuilderLengthMethods
) –New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
NumberOfTurns¶
-
HelixBuilder.
NumberOfTurns
¶ Returns or sets the number of turns
-------------------------------------
Getter Method
Signature
NumberOfTurns()
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NumberOfTurns(numberOfTurns)
Parameters: numberOfTurns (str) – New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
OrientationOption¶
-
HelixBuilder.
OrientationOption
¶ Returns or sets the orientation option
-------------------------------------
Getter Method
Signature
OrientationOption()
Returns: Return type: NXOpen.Features.HelixBuilderOrientationOptions
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OrientationOption(orientationOption)
Parameters: orientationOption ( NXOpen.Features.HelixBuilderOrientationOptions
) –New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
PitchLaw¶
-
HelixBuilder.
PitchLaw
¶ Returns the pitch
-------------------------------------
Getter Method
Signature
PitchLaw()
Returns: Return type: NXOpen.GeometricUtilities.LawBuilder
New in version NX8.5.0.
License requirements: None.
SizeLaw¶
-
HelixBuilder.
SizeLaw
¶ Returns the size law
-------------------------------------
Getter Method
Signature
SizeLaw()
Returns: Return type: NXOpen.GeometricUtilities.LawBuilder
New in version NX8.5.0.
License requirements: None.
SizeOption¶
-
HelixBuilder.
SizeOption
¶ Returns or sets the size option
-------------------------------------
Getter Method
Signature
SizeOption()
Returns: Return type: NXOpen.Features.HelixBuilderSizeOptions
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SizeOption(sizeOption)
Parameters: sizeOption ( NXOpen.Features.HelixBuilderSizeOptions
) –New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Spine¶
-
HelixBuilder.
Spine
¶ Returns the length spine
-------------------------------------
Getter Method
Signature
Spine()
Returns: Return type: NXOpen.Section
New in version NX8.5.0.
License requirements: None.
StartAngle¶
-
HelixBuilder.
StartAngle
¶ Returns the start angle
-------------------------------------
Getter Method
Signature
StartAngle()
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
StartLimit¶
-
HelixBuilder.
StartLimit
¶ Returns the start limit
-------------------------------------
Getter Method
Signature
StartLimit()
Returns: Return type: NXOpen.GeometricUtilities.OnPathDimensionBuilder
New in version NX8.5.0.
License requirements: None.
TurnDirection¶
-
HelixBuilder.
TurnDirection
¶ Returns or sets the turn direction
-------------------------------------
Getter Method
Signature
TurnDirection()
Returns: Return type: NXOpen.Features.HelixBuilderTurnDirections
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TurnDirection(turnDirection)
Parameters: turnDirection ( NXOpen.Features.HelixBuilderTurnDirections
) –New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Type¶
-
HelixBuilder.
Type
¶ Returns or sets the type
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.Features.HelixBuilderTypes
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(type)
Parameters: type ( NXOpen.Features.HelixBuilderTypes
) –New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Method Detail¶
Evaluate¶
-
HelixBuilder.
Evaluate
¶ Evaluates the curve
Signature
Evaluate()
New in version NX8.5.0.
License requirements: features_modeling (“FEATURES MODELING”)
Validate¶
-
HelixBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.