CustomIntegerAttribute Class¶
-
class
NXOpen.Features.
CustomIntegerAttribute
¶ Bases:
NXOpen.Features.CustomAttribute
Represents a
Features.CustomIntegerAttribute
classAn instance of this class can be obtained from
NXOpen.Features.CustomAttributeCollection.CreateCustomIntegerAttribute()
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
Name | Returns or sets the custom attribute name |
TypeValue | Returns the custom attribute type value |
Value | Returns or sets the integer value in the attribute |
Methods¶
Method | Description |
---|---|
AddProperty | The custom attribute add property |
Dispose | Frees the memory associated with this object. |
GetProperties | The custom attribute get all properties @return |
HasProperty | The custom attribute does property exist on attribute @return |
RemoveProperty | The custom attribute remove property |
Property Detail¶
Value¶
-
CustomIntegerAttribute.
Value
¶ Returns or sets the integer value in the attribute
-------------------------------------
Getter Method
Signature
Value()
Returns: Return type: int New in version NX11.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
-------------------------------------
Setter Method
Signature
Value(intValue)
Parameters: intValue (int) – New in version NX11.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)