PaintFacetBodyBuilder Class¶
-
class
NXOpen.Facet.
PaintFacetBodyBuilder
¶ Bases:
NXOpen.Builder
This class manages the color painting on a facet body.
To create a new instance of this class, use
NXOpen.Facet.FacetModelingCollection.CreatePaintFacetBodyBuilder()
Default values.
Property Value PaintBrushSize.Value 20.0 (millimeters part), 1.0 (inches part) New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
InheritBodyColorPick | Returns the inherit color pick. |
InheritColorPick | Returns the inherit color pick |
PaintBrush | Returns the paint brush |
PaintBrushSize | Returns the paint brush size |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetPaintBrushColor | Returns the paint brush color @return Array of 3 RGB values, each between 0 and 1 |
PaintBodiesBackgroundColor | Paints facets background color. |
PaintFacetsBackGroundColor | Paints facets background color |
SetPaintBrushColor | Sets the paint brush color |
SetupBodyColorData | Setup color data. |
SetupColorData | Setup color data |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
InheritBodyColorPick¶
-
PaintFacetBodyBuilder.
InheritBodyColorPick
¶ Returns the inherit color pick.
Inputs to this command can be convergent objects.
-------------------------------------
Getter Method
Signature
InheritBodyColorPick()
Returns: Return type: NXOpen.SelectDisplayableObject
New in version NX11.0.0.
License requirements: None.
InheritColorPick¶
-
PaintFacetBodyBuilder.
InheritColorPick
¶ Returns the inherit color pick
-------------------------------------
Getter Method
Signature
InheritColorPick()
Returns: Return type: NXOpen.Facet.SelectFacetedBody
New in version NX10.0.0.
Deprecated since version NX11.0.0: Use
NXOpen.Facet.PaintFacetBodyBuilder.InheritBodyColorPick()
instead.License requirements: None.
PaintBrush¶
-
PaintFacetBodyBuilder.
PaintBrush
¶ Returns the paint brush
-------------------------------------
Getter Method
Signature
PaintBrush()
Returns: Return type: NXOpen.Facet.PaintBrushBuilder
New in version NX10.0.0.
License requirements: None.
PaintBrushSize¶
-
PaintFacetBodyBuilder.
PaintBrushSize
¶ Returns the paint brush size
-------------------------------------
Getter Method
Signature
PaintBrushSize()
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
Method Detail¶
GetPaintBrushColor¶
-
PaintFacetBodyBuilder.
GetPaintBrushColor
¶ Returns the paint brush color
Signature
GetPaintBrushColor()
Returns: Array of 3 RGB values, each between 0 and 1 Return type: list of float New in version NX10.0.0.
License requirements: None.
PaintBodiesBackgroundColor¶
-
PaintFacetBodyBuilder.
PaintBodiesBackgroundColor
¶ Paints facets background color.
Inputs to this command can be convergent objects.
Signature
PaintBodiesBackgroundColor(bodies)
Parameters: bodies (list of NXOpen.DisplayableObject
) – Bodies to be painted with background colorNew in version NX11.0.0.
License requirements: None.
PaintFacetsBackGroundColor¶
-
PaintFacetBodyBuilder.
PaintFacetsBackGroundColor
¶ Paints facets background color
Signature
PaintFacetsBackGroundColor(facets)
Parameters: facets (list of NXOpen.Facet.FacetedBody
) – Facets to be painted with background colorNew in version NX10.0.0.
Deprecated since version NX11.0.0: Use
NXOpen.Facet.PaintFacetBodyBuilder.PaintBodiesBackgroundColor()
instead.License requirements: None.
SetPaintBrushColor¶
-
PaintFacetBodyBuilder.
SetPaintBrushColor
¶ Sets the paint brush color
Signature
SetPaintBrushColor(paintBrushColor)
Parameters: paintBrushColor (list of float) – Array of 3 RGB values, each between 0 and 1 New in version NX10.0.0.
License requirements: None.
SetupBodyColorData¶
-
PaintFacetBodyBuilder.
SetupBodyColorData
¶ Setup color data.
Inputs to this command can be convergent objects.
Signature
SetupBodyColorData(bodies)
Parameters: bodies (list of NXOpen.DisplayableObject
) – Bodies that need color data for editNew in version NX11.0.0.
License requirements: None.
SetupColorData¶
-
PaintFacetBodyBuilder.
SetupColorData
¶ Setup color data
Signature
SetupColorData(facets)
Parameters: facets (list of NXOpen.Facet.FacetedBody
) – Facets that need color data for editNew in version NX10.0.0.
Deprecated since version NX11.0.0: Use
NXOpen.Facet.PaintFacetBodyBuilder.SetupBodyColorData()
instead.License requirements: None.
Validate¶
-
PaintFacetBodyBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.