RibChildBuilder Class¶
-
class
NXOpen.Die.
RibChildBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a Die Rib Child sub feature.
This sub feature is created via the main feature builder.
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
AdjustedThickness | Returns or sets the adjusted thickness of the die rib. |
Angle | Returns or sets the angle of the die rib. |
Bottom | Returns or sets the bottom limit geometry of the die rib. |
BottomEnd | Returns or sets the bottom end limit geometry of the die rib. |
BottomHorizontalOffset | Returns or sets the bottom horizontal offset of the die rib. |
BottomLimitOffset | Returns or sets the bottom limit offset of the die rib. |
BottomVerticalOffset | Returns or sets the bottom vertical offset of the die rib. |
BuildStatus | Returns the build status of the die rib. |
CenterlineXyOffset | Returns or sets the centerline xy offset of the die rib. |
DesignStatus | Returns or sets the design status of the die rib, if true the rib will be built into the model, if false it will not. |
DisplayStatus | Returns or sets the display status of the die rib, if true input data to the rib will be displayed, if false the input data will not be displayed. |
Height | Returns or sets the height of the die rib. |
LccMinWidth | Returns or sets the lightening core mininum width of the die rib. |
LighteningCore | Returns or sets the lightening core switch of the die rib, if true the lightening core will be built into the rib, if false it will not. |
LighteningCoreClearance | Returns or sets the lightening core clearance of the die rib. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
Rectangular | Returns or sets the rectangular switch of the die rib, if true the lightening core will be rectangular, if false it will follow the shape of the rib. |
Start | Returns or sets the start limit geometry of the die rib. |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Thickness | Returns or sets the thickness of the die rib. |
Top | Returns or sets the top limit geometry of the die rib. |
TopEnd | Returns or sets the top end limit geometry of the die rib. |
TopHorizontalOffset | Returns or sets the top horizontal offset of the die rib. |
TopLimitOffset | Returns or sets the top limit offset of the die rib. |
TopVerticalOffset | Returns or sets the top vertical offset of the die rib. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCenterline | Gets the centerline of the rib. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetCenterline | Sets the centerline of the rib. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AdjustedThickness¶
-
RibChildBuilder.
AdjustedThickness
¶ Returns or sets the adjusted thickness of the die rib.
-------------------------------------
Getter Method
Signature
AdjustedThickness()
Returns: Return type: float New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
AdjustedThickness(adjustedThickness)
Parameters: adjustedThickness (float) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
Angle¶
-
RibChildBuilder.
Angle
¶ Returns or sets the angle of the die rib.
-------------------------------------
Getter Method
Signature
Angle()
Returns: Return type: float New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
Angle(angle)
Parameters: angle (float) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
Bottom¶
-
RibChildBuilder.
Bottom
¶ Returns or sets the bottom limit geometry of the die rib.
-------------------------------------
Getter Method
Signature
Bottom()
Returns: Return type: NXOpen.IOrientation
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
Bottom(bottom)
Parameters: bottom ( NXOpen.IOrientation
) –New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
BottomEnd¶
-
RibChildBuilder.
BottomEnd
¶ Returns or sets the bottom end limit geometry of the die rib.
-------------------------------------
Getter Method
Signature
BottomEnd()
Returns: Return type: NXOpen.IOrientation
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
BottomEnd(bottomEnd)
Parameters: bottomEnd ( NXOpen.IOrientation
) –New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
BottomHorizontalOffset¶
-
RibChildBuilder.
BottomHorizontalOffset
¶ Returns or sets the bottom horizontal offset of the die rib.
-------------------------------------
Getter Method
Signature
BottomHorizontalOffset()
Returns: Return type: float New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
BottomHorizontalOffset(bottomHorizontalOffset)
Parameters: bottomHorizontalOffset (float) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
BottomLimitOffset¶
-
RibChildBuilder.
BottomLimitOffset
¶ Returns or sets the bottom limit offset of the die rib.
-------------------------------------
Getter Method
Signature
BottomLimitOffset()
Returns: Return type: float New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
BottomLimitOffset(bottomLimitOffset)
Parameters: bottomLimitOffset (float) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
BottomVerticalOffset¶
-
RibChildBuilder.
BottomVerticalOffset
¶ Returns or sets the bottom vertical offset of the die rib.
-------------------------------------
Getter Method
Signature
BottomVerticalOffset()
Returns: Return type: float New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
BottomVerticalOffset(bottomVerticalOffset)
Parameters: bottomVerticalOffset (float) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
BuildStatus¶
-
RibChildBuilder.
BuildStatus
¶ Returns the build status of the die rib.
-------------------------------------
Getter Method
Signature
BuildStatus()
Returns: Return type: NXOpen.Die.DieBuildStatusOption
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
CenterlineXyOffset¶
-
RibChildBuilder.
CenterlineXyOffset
¶ Returns or sets the centerline xy offset of the die rib.
-------------------------------------
Getter Method
Signature
CenterlineXyOffset()
Returns: Return type: float New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
CenterlineXyOffset(centerlineXyOffset)
Parameters: centerlineXyOffset (float) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
DesignStatus¶
-
RibChildBuilder.
DesignStatus
¶ Returns or sets the design status of the die rib, if true the rib will be built into the model, if false it will not.
-------------------------------------
Getter Method
Signature
DesignStatus()
Returns: Return type: bool New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
DesignStatus(designStatus)
Parameters: designStatus (bool) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
DisplayStatus¶
-
RibChildBuilder.
DisplayStatus
¶ Returns or sets the display status of the die rib, if true input data to the rib will be displayed, if false the input data will not be displayed.
-------------------------------------
Getter Method
Signature
DisplayStatus()
Returns: Return type: bool New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
DisplayStatus(displayStatus)
Parameters: displayStatus (bool) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
Height¶
-
RibChildBuilder.
Height
¶ Returns or sets the height of the die rib.
-------------------------------------
Getter Method
Signature
Height()
Returns: Return type: float New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
Height(height)
Parameters: height (float) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
LccMinWidth¶
-
RibChildBuilder.
LccMinWidth
¶ Returns or sets the lightening core mininum width of the die rib.
-------------------------------------
Getter Method
Signature
LccMinWidth()
Returns: Return type: float New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
LccMinWidth(lccMinWidth)
Parameters: lccMinWidth (float) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
LighteningCore¶
-
RibChildBuilder.
LighteningCore
¶ Returns or sets the lightening core switch of the die rib, if true the lightening core will be built into the rib, if false it will not.
-------------------------------------
Getter Method
Signature
LighteningCore()
Returns: Return type: bool New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
LighteningCore(lighteningCore)
Parameters: lighteningCore (bool) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
LighteningCoreClearance¶
-
RibChildBuilder.
LighteningCoreClearance
¶ Returns or sets the lightening core clearance of the die rib.
-------------------------------------
Getter Method
Signature
LighteningCoreClearance()
Returns: Return type: float New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
LighteningCoreClearance(lighteningCoreClearance)
Parameters: lighteningCoreClearance (float) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
Rectangular¶
-
RibChildBuilder.
Rectangular
¶ Returns or sets the rectangular switch of the die rib, if true the lightening core will be rectangular, if false it will follow the shape of the rib.
-------------------------------------
Getter Method
Signature
Rectangular()
Returns: Return type: bool New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
Rectangular(rectangular)
Parameters: rectangular (bool) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
Start¶
-
RibChildBuilder.
Start
¶ Returns or sets the start limit geometry of the die rib.
-------------------------------------
Getter Method
Signature
Start()
Returns: Return type: NXOpen.IOrientation
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
Start(start)
Parameters: start ( NXOpen.IOrientation
) –New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
Thickness¶
-
RibChildBuilder.
Thickness
¶ Returns or sets the thickness of the die rib.
-------------------------------------
Getter Method
Signature
Thickness()
Returns: Return type: float New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
Thickness(thickness)
Parameters: thickness (float) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
Top¶
-
RibChildBuilder.
Top
¶ Returns or sets the top limit geometry of the die rib.
-------------------------------------
Getter Method
Signature
Top()
Returns: Return type: NXOpen.IOrientation
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
Top(top)
Parameters: top ( NXOpen.IOrientation
) –New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
TopEnd¶
-
RibChildBuilder.
TopEnd
¶ Returns or sets the top end limit geometry of the die rib.
-------------------------------------
Getter Method
Signature
TopEnd()
Returns: Return type: NXOpen.IOrientation
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
TopEnd(topEnd)
Parameters: topEnd ( NXOpen.IOrientation
) –New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
TopHorizontalOffset¶
-
RibChildBuilder.
TopHorizontalOffset
¶ Returns or sets the top horizontal offset of the die rib.
-------------------------------------
Getter Method
Signature
TopHorizontalOffset()
Returns: Return type: float New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
TopHorizontalOffset(topHorizontalOffset)
Parameters: topHorizontalOffset (float) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
TopLimitOffset¶
-
RibChildBuilder.
TopLimitOffset
¶ Returns or sets the top limit offset of the die rib.
-------------------------------------
Getter Method
Signature
TopLimitOffset()
Returns: Return type: float New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
TopLimitOffset(topLimitOffset)
Parameters: topLimitOffset (float) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
TopVerticalOffset¶
-
RibChildBuilder.
TopVerticalOffset
¶ Returns or sets the top vertical offset of the die rib.
-------------------------------------
Getter Method
Signature
TopVerticalOffset()
Returns: Return type: float New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
TopVerticalOffset(topVerticalOffset)
Parameters: topVerticalOffset (float) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
Method Detail¶
GetCenterline¶
-
RibChildBuilder.
GetCenterline
¶ Gets the centerline of the rib.
Signature
GetCenterline()
Returns: a tuple Return type: A tuple consisting of (profileEntries, direction). profileEntries is a list of NXOpen.IProfile
. The profile entries, will be curves, edges, faces, sketches or curve features. direction is aNXOpen.Die.DirectionOption
. Profile direction.New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetCenterline¶
-
RibChildBuilder.
SetCenterline
¶ Sets the centerline of the rib.
Signature
SetCenterline(direction, profileEntries)
Parameters: - direction (
NXOpen.Die.DirectionOption
) – Profile direction. - profileEntries (list of
NXOpen.IProfile
) – The profile entries, can be curves, edges, faces, sketches or curve features.
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
- direction (
Validate¶
-
RibChildBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.