HandlingCoreParentBuilder Class

class NXOpen.Die.HandlingCoreParentBuilder

Bases: NXOpen.Features.FeatureBuilder

Represents a Die Handling Core Parent sub feature.

This sub feature is created via the main feature builder.

New in version NX4.0.0.

Properties

Property Description
BuildStatus Returns the build status of handling cores.
Clearance Returns or sets the clearance of handling cores.
Depth Returns or sets the depth of handling cores.
DesignStatus Returns or sets the design status of handling cores, if true the handling cores will be built into the model, if false they will not.
DisplayStatus Returns or sets the display status of handling cores, if true input data to the handling cores will be displayed, if false the input data will not be displayed.
Height Returns or sets the height of handling cores.
ParentFeatureInternal Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal
PatchSolutionFlag Returns or sets the patch solution flag
PatchSurfaceFilename Returns or sets the patch surface filename
SurroundingPatchSurfaceFilename Returns or sets the surrounding patch surface filename
Tag Returns the Tag for this object.
Width Returns or sets the width of handling cores.

Methods

Method Description
Commit Commits any edits that have been applied to the builder.
CommitFeature Commits the feature parameters and creates the feature @return
CreateChild Creates a child handling core.
DeleteChild Deletes a child handling core.
Destroy Deletes the builder, and cleans up any objects created by the builder.
GetChildren Outputs the child handling cores.
GetCommittedObjects For builders that create more than one object, this method returns the objects that are created by commit.
GetFeature Returns the feature currently being edited by this builder.
GetObject Returns the object currently being edited by this builder.
HideInternalParentFeatureAfterEdit Re-suppress an internal parent feature (a slave feature) after it has been edited.
SetParentFeatureInternal Set the parent features which would be internal or slaves to the feature being created or commited
ShowInternalParentFeatureForEdit Unsuppress an internal parent feature (a slave feature) so it can be edited.
ShowResults Updates the model to reflect the result of an edit to the model for all builders that support showing results.
UnsetParentFeatureInternal Set the internal parent feature of the feature being edited to external
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Property Detail

BuildStatus

HandlingCoreParentBuilder.BuildStatus

Returns the build status of handling cores.

-------------------------------------

Getter Method

Signature BuildStatus()

Returns:
Return type:NXOpen.Die.DieBuildStatusOption

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

Clearance

HandlingCoreParentBuilder.Clearance

Returns or sets the clearance of handling cores.

-------------------------------------

Getter Method

Signature Clearance()

Returns:
Return type:float

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

-------------------------------------

Setter Method

Signature Clearance(clearance)

Parameters:clearance (float) –

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

Depth

HandlingCoreParentBuilder.Depth

Returns or sets the depth of handling cores.

-------------------------------------

Getter Method

Signature Depth()

Returns:
Return type:float

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

-------------------------------------

Setter Method

Signature Depth(depth)

Parameters:depth (float) –

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

DesignStatus

HandlingCoreParentBuilder.DesignStatus

Returns or sets the design status of handling cores, if true the handling cores will be built into the model, if false they will not.

-------------------------------------

Getter Method

Signature DesignStatus()

Returns:
Return type:bool

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

-------------------------------------

Setter Method

Signature DesignStatus(designStatus)

Parameters:designStatus (bool) –

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

DisplayStatus

HandlingCoreParentBuilder.DisplayStatus

Returns or sets the display status of handling cores, if true input data to the handling cores will be displayed, if false the input data will not be displayed.

-------------------------------------

Getter Method

Signature DisplayStatus()

Returns:
Return type:bool

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

-------------------------------------

Setter Method

Signature DisplayStatus(displayStatus)

Parameters:displayStatus (bool) –

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

Height

HandlingCoreParentBuilder.Height

Returns or sets the height of handling cores.

-------------------------------------

Getter Method

Signature Height()

Returns:
Return type:float

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

-------------------------------------

Setter Method

Signature Height(height)

Parameters:height (float) –

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

Width

HandlingCoreParentBuilder.Width

Returns or sets the width of handling cores.

-------------------------------------

Getter Method

Signature Width()

Returns:
Return type:float

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

-------------------------------------

Setter Method

Signature Width(width)

Parameters:width (float) –

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

Method Detail

CreateChild

HandlingCoreParentBuilder.CreateChild

Creates a child handling core.

Signature CreateChild()

Returns:
Return type:NXOpen.Die.HandlingCoreChildBuilder

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

DeleteChild

HandlingCoreParentBuilder.DeleteChild

Deletes a child handling core.

Signature DeleteChild(diehandlingcorechild)

Parameters:diehandlingcorechild (NXOpen.Die.HandlingCoreChildBuilder) –

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

GetChildren

HandlingCoreParentBuilder.GetChildren

Outputs the child handling cores.

Signature GetChildren()

Returns:The child handling cores.
Return type:list of NXOpen.Die.HandlingCoreChildBuilder

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

Validate

HandlingCoreParentBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.