HandlingCoreChildBuilder Class

class NXOpen.Die.HandlingCoreChildBuilder

Bases: NXOpen.Features.FeatureBuilder

Represents a Die Handling Core Child sub feature.

This sub feature is created via the main feature builder.

New in version NX4.0.0.

Properties

Property Description
BuildStatus Returns the build status of the handling core.
Center Returns or sets the center of the handling core.
Clearance Returns or sets the clearance of the handling core.
CoreOrientation Returns or sets the core orientation of the handling core.
Depth Returns or sets the depth of the handling core.
DesignStatus Returns or sets the design status of the handling core, if true the handling core will be built into the model, if false it will not.
DisplayStatus Returns or sets the display status of the handling core, if true input data to the handling core will be displayed, if false the input data will not be displayed.
Height Returns or sets the height of the handling core.
ParentFeatureInternal Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal
PatchSolutionFlag Returns or sets the patch solution flag
PatchSurfaceFilename Returns or sets the patch surface filename
ReverseOrientation Returns or sets the value to reverse the orientation of the core plane, if true the handling core orientation normal will be reversed, if false it will not.
SurroundingPatchSurfaceFilename Returns or sets the surrounding patch surface filename
Tag Returns the Tag for this object.
Width Returns or sets the width of the handling core.

Methods

Method Description
Commit Commits any edits that have been applied to the builder.
CommitFeature Commits the feature parameters and creates the feature @return
Destroy Deletes the builder, and cleans up any objects created by the builder.
GetCommittedObjects For builders that create more than one object, this method returns the objects that are created by commit.
GetFeature Returns the feature currently being edited by this builder.
GetObject Returns the object currently being edited by this builder.
HideInternalParentFeatureAfterEdit Re-suppress an internal parent feature (a slave feature) after it has been edited.
SetParentFeatureInternal Set the parent features which would be internal or slaves to the feature being created or commited
ShowInternalParentFeatureForEdit Unsuppress an internal parent feature (a slave feature) so it can be edited.
ShowResults Updates the model to reflect the result of an edit to the model for all builders that support showing results.
TranslateCenter Translates the center of the die handling core by the specified amount.
UnsetParentFeatureInternal Set the internal parent feature of the feature being edited to external
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Property Detail

BuildStatus

HandlingCoreChildBuilder.BuildStatus

Returns the build status of the handling core.

-------------------------------------

Getter Method

Signature BuildStatus()

Returns:
Return type:NXOpen.Die.DieBuildStatusOption

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

Center

HandlingCoreChildBuilder.Center

Returns or sets the center of the handling core.

-------------------------------------

Getter Method

Signature Center()

Returns:
Return type:NXOpen.ILocation

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

-------------------------------------

Setter Method

Signature Center(center)

Parameters:center (NXOpen.ILocation) –

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

Clearance

HandlingCoreChildBuilder.Clearance

Returns or sets the clearance of the handling core.

-------------------------------------

Getter Method

Signature Clearance()

Returns:
Return type:float

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

-------------------------------------

Setter Method

Signature Clearance(clearance)

Parameters:clearance (float) –

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

CoreOrientation

HandlingCoreChildBuilder.CoreOrientation

Returns or sets the core orientation of the handling core.

-------------------------------------

Getter Method

Signature CoreOrientation()

Returns:
Return type:NXOpen.ISurface

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

-------------------------------------

Setter Method

Signature CoreOrientation(coreOrientation)

Parameters:coreOrientation (NXOpen.ISurface) –

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

Depth

HandlingCoreChildBuilder.Depth

Returns or sets the depth of the handling core.

-------------------------------------

Getter Method

Signature Depth()

Returns:
Return type:float

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

-------------------------------------

Setter Method

Signature Depth(depth)

Parameters:depth (float) –

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

DesignStatus

HandlingCoreChildBuilder.DesignStatus

Returns or sets the design status of the handling core, if true the handling core will be built into the model, if false it will not.

-------------------------------------

Getter Method

Signature DesignStatus()

Returns:
Return type:bool

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

-------------------------------------

Setter Method

Signature DesignStatus(designStatus)

Parameters:designStatus (bool) –

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

DisplayStatus

HandlingCoreChildBuilder.DisplayStatus

Returns or sets the display status of the handling core, if true input data to the handling core will be displayed, if false the input data will not be displayed.

-------------------------------------

Getter Method

Signature DisplayStatus()

Returns:
Return type:bool

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

-------------------------------------

Setter Method

Signature DisplayStatus(displayStatus)

Parameters:displayStatus (bool) –

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

Height

HandlingCoreChildBuilder.Height

Returns or sets the height of the handling core.

-------------------------------------

Getter Method

Signature Height()

Returns:
Return type:float

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

-------------------------------------

Setter Method

Signature Height(height)

Parameters:height (float) –

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

ReverseOrientation

HandlingCoreChildBuilder.ReverseOrientation

Returns or sets the value to reverse the orientation of the core plane, if true the handling core orientation normal will be reversed, if false it will not.

-------------------------------------

Getter Method

Signature ReverseOrientation()

Returns:
Return type:bool

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

-------------------------------------

Setter Method

Signature ReverseOrientation(reverseOrientation)

Parameters:reverseOrientation (bool) –

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

Width

HandlingCoreChildBuilder.Width

Returns or sets the width of the handling core.

-------------------------------------

Getter Method

Signature Width()

Returns:
Return type:float

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

-------------------------------------

Setter Method

Signature Width(width)

Parameters:width (float) –

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

Method Detail

TranslateCenter

HandlingCoreChildBuilder.TranslateCenter

Translates the center of the die handling core by the specified amount.

Signature TranslateCenter(translateDist)

Parameters:translateDist (NXOpen.Vector3d) – A scaled vector indicating the distance to translate

New in version NX5.0.0.

License requirements: ug_die_design (“Die Design”)

Validate

HandlingCoreChildBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.