WorkInstructionOutputBuilder Class¶
-
class
NXOpen.CAM.
WorkInstructionOutputBuilder
¶ Bases:
NXOpen.Builder
Represents the builder for Work Instruction Output.
This class is used to publish work instructions for the end user. To create a new instance of this class, use
NXOpen.CAM.CAMSetup.CreateWorkInstructionOutputBuilder()
New in version NX9.0.3.
Properties¶
Property | Description |
---|---|
OpenFile | Returns or sets the open file |
OutputFile | Returns or sets the output file |
OutputFormat | Returns or sets the output format |
PageOrientation | Returns or sets the page orientation |
PageSize | Returns or sets the page size |
ScaleFactor | Returns or sets the scale factor |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
Publish | Publish the Work Instructions |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
WorkInstructionOutputBuilderOutputFormatType Enumeration | the output format type |
WorkInstructionOutputBuilderPageOrientationType Enumeration | the page orientation type |
WorkInstructionOutputBuilderPageSizeType Enumeration | the page size type |
Property Detail¶
OpenFile¶
-
WorkInstructionOutputBuilder.
OpenFile
¶ Returns or sets the open file
-------------------------------------
Getter Method
Signature
OpenFile()
Returns: Return type: bool New in version NX9.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
OpenFile(openFile)
Parameters: openFile (bool) – New in version NX9.0.3.
License requirements: nx_wi_authoring (” NX Work Instruction Authoring”)
OutputFile¶
-
WorkInstructionOutputBuilder.
OutputFile
¶ Returns or sets the output file
-------------------------------------
Getter Method
Signature
OutputFile()
Returns: Return type: str New in version NX9.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
OutputFile(filename)
Parameters: filename (str) – New in version NX9.0.3.
License requirements: nx_wi_authoring (” NX Work Instruction Authoring”)
OutputFormat¶
-
WorkInstructionOutputBuilder.
OutputFormat
¶ Returns or sets the output format
-------------------------------------
Getter Method
Signature
OutputFormat()
Returns: Return type: NXOpen.CAM.WorkInstructionOutputBuilderOutputFormatType
New in version NX9.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
OutputFormat(format)
Parameters: format ( NXOpen.CAM.WorkInstructionOutputBuilderOutputFormatType
) –New in version NX9.0.3.
License requirements: nx_wi_authoring (” NX Work Instruction Authoring”)
PageOrientation¶
-
WorkInstructionOutputBuilder.
PageOrientation
¶ Returns or sets the page orientation
-------------------------------------
Getter Method
Signature
PageOrientation()
Returns: Return type: NXOpen.CAM.WorkInstructionOutputBuilderPageOrientationType
New in version NX9.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
PageOrientation(pageOrientation)
Parameters: pageOrientation ( NXOpen.CAM.WorkInstructionOutputBuilderPageOrientationType
) –New in version NX9.0.3.
License requirements: nx_wi_authoring (” NX Work Instruction Authoring”)
PageSize¶
-
WorkInstructionOutputBuilder.
PageSize
¶ Returns or sets the page size
-------------------------------------
Getter Method
Signature
PageSize()
Returns: Return type: NXOpen.CAM.WorkInstructionOutputBuilderPageSizeType
New in version NX9.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
PageSize(pageSize)
Parameters: pageSize ( NXOpen.CAM.WorkInstructionOutputBuilderPageSizeType
) –New in version NX9.0.3.
License requirements: nx_wi_authoring (” NX Work Instruction Authoring”)
ScaleFactor¶
-
WorkInstructionOutputBuilder.
ScaleFactor
¶ Returns or sets the scale factor
-------------------------------------
Getter Method
Signature
ScaleFactor()
Returns: Return type: float New in version NX9.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
ScaleFactor(scaleFactor)
Parameters: scaleFactor (float) – New in version NX9.0.3.
License requirements: nx_wi_authoring (” NX Work Instruction Authoring”)
Method Detail¶
Publish¶
-
WorkInstructionOutputBuilder.
Publish
¶ Publish the Work Instructions
Signature
Publish(objects, firstSelObj, currentView)
Parameters: - objects (list of
NXOpen.CAM.CAMObject
) – array of objects - firstSelObj (
NXOpen.CAM.CAMObject
) – - currentView (int) – CAM_SETUP_view
New in version NX9.0.3.
License requirements: nx_wi_authoring (” NX Work Instruction Authoring”)
- objects (list of
Validate¶
-
WorkInstructionOutputBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.