WorkInstructionOutputBuilderPageSizeType Enumeration¶
NXOpen.CAM.WorkInstructionOutputBuilder.PageSizeType is an alias for NXOpen.CAM.WorkInstructionOutputBuilderPageSizeType
-
class
NXOpen.CAM.
WorkInstructionOutputBuilderPageSizeType
¶ Bases:
object
the page size type
Enum Members
Enum Member Enum Member Description A0 A1 A2 A3 A4 B1 B2 B3 B4 B5 Executive Folio Legal Letter Tabloid -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-