WedmStepoverBuilder Class¶
-
class
NXOpen.CAM.
WedmStepoverBuilder
¶ Bases:
NXOpen.CAM.StepoverBuilder
Represents a
NXOpen.CAM.WedmStepoverBuilder
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
AdditionalPasses | Returns or sets the number of additional passes |
Angular | Returns or sets the angular |
ApplyOn | Returns or sets the apply on part option |
BlankContourDepth | Returns the Stepover Depth Builder |
BlankContourNoLevels | Returns or sets the number of levels |
DistanceBuilder | Returns the distance (inheritable tool dependent) |
DistanceMaximumBuilder | Returns the distance maximum(inheritable tool dependent) |
DistanceMinimumBuilder | Returns the distance minimum(inheritable tool dependent) |
FirstDistance | Returns the First Distance |
HorizontalLimitBuilder | Returns the horizontal limit (inheritable tool dependent) |
InheritableDistance | Returns the distance (inheritable double) |
MaximumAverage | Returns or sets the variable average maximum value |
MaximumAverageBuilder | Returns the variable average maximum builder |
MaximumAverageOnlyBuilder | Returns the variable average maximum only builder |
MaximumBuilder | Returns the maximum builder |
MaximumPercentBuilder | Returns the maximum percent of remaining |
MinimumAverage | Returns or sets the variable average minimum value |
MinimumAverageBuilder | Returns the variable average minimum builder |
MinimumDistance | Returns the Minimum Distance |
MinimumPercentBuilder | Returns the minimum percent of remaining |
MultipleBuilder | Returns the multiple builder |
NumberAtFirstDirection | Returns or sets the number of stepovers at first direction |
NumberAtSecondDirection | Returns or sets the number of stepovers at second direction |
NumberOfStepovers | Returns or sets the number of stepovers |
PercentFluteLength | Returns the percent flute of length |
PercentOfDegression | Returns or sets the Percent of Degression |
PercentOfRemainingBuilder | Returns the percent of remaining |
PercentThreadLength | Returns the percent thread length |
PercentToolFlatBuilder | Returns the percent tool flat |
PercentWireBuilder | Returns the % wire (inheritable tool dependent) |
ScallopBuilder | Returns the scallop height |
StepoverType | Returns or sets the stepover type |
StepoverTypeType | Returns or sets the stepover item type |
StockPerPassBuilder | Returns the stock per pass |
Tag | Returns the Tag for this object. |
UserDefined | Returns the user defined builder |
ValueOfDegression | Returns the Value of Degression |
VariableMaximumBuilder | Returns the variable maximum builder |
VariableMaximumOnlyBuilder | Returns the variable maximum only builder |
VariableMinimumBuilder | Returns the variable minimum builder |
VerticalLimitBuilder | Returns the vertical limit (inheritable tool dependent) |
Methods¶
Property Detail¶
StepoverTypeType¶
-
WedmStepoverBuilder.
StepoverTypeType
¶ Returns or sets the stepover item type
-------------------------------------
Getter Method
Signature
StepoverTypeType()
Returns: the stepover type Return type: NXOpen.CAM.StepoverBuilderStepoverTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StepoverTypeType(newValue)
Parameters: newValue ( NXOpen.CAM.StepoverBuilderStepoverTypes
) – the stepover typeNew in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)