StepoverBuilderStepoverTypes Enumeration¶
NXOpen.CAM.StepoverBuilder.StepoverTypes is an alias for NXOpen.CAM.StepoverBuilderStepoverTypes
-
class
NXOpen.CAM.
StepoverBuilderStepoverTypes
¶ Bases:
object
stepover options
New in version NX6.0.0.
Enum Members
Enum Member Enum Member Description NotSet NoneConstant ConstantScallop ScallopPercentToolFlat % Tool FlatMultiple MultipleNumber Number of stepoversMaximum Maximum StepoverAngular AngularVariableAverage Variable AverageVariableMaximum Variable MaximumUseCutDepth Use Depth Of CutPercentRemaining Percent Of RemainingPercentWire % WireStockPerPass Stock Per PassPercentThreadLength Percent Thread LengthExact ExactPercentFluteLength Percent Flute LengthBlankContourConstant Depth and Number of levelsDegression DegressionPercentDegression % DegressionUserDefined User Defined-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-