WedmNocoreGeomBuilder Class¶
-
class
NXOpen.CAM.
WedmNocoreGeomBuilder
¶ Bases:
NXOpen.CAM.WedmBasedGeomBuilder
Represents a WedmNocoreGeom Builder
To create a new instance of this class, use
NXOpen.CAM.NCGroupCollection.CreateWedmNocoreGeomBuilder()
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
BackburnPasses | Returns or sets the Backburn Passes |
CustomBoundaryDataList | Returns the Custom Boundary Data List |
CutDirection | Returns or sets the Cut Direction |
CutoffDistance | Returns or sets the Cutoff Distance |
CutoffFlag | Returns or sets the Cutoff Flag |
CutoffStock | Returns or sets the Cutoff Stock |
CycleEvent | Returns the cycle event |
CycleTable | Returns the cycle |
FinishPasses | Returns or sets the Finish Passes |
FromPoint | Returns or sets the From Point |
FromPointStatus | Returns or sets the From Point Status |
FromPointToolAxis | Returns or sets the From Point Tool Axis |
GoHomePoint | Returns or sets the Go Home Point |
GoHomePointStatus | Returns or sets the Go Home Point Status |
GoHomePointToolAxis | Returns or sets the Go Home Point Tool Axis |
Intol | Returns or sets the intol value |
LayoutCiBuilder | Returns the Save Layer/Layout builder |
LeadInPoint | Returns or sets the Lead In Point |
LeadInPointStatus | Returns or sets the Lead In Point Status |
LeadOutPointStatus | Returns or sets the Lead Out Point Status |
LowerPlane | Returns or sets the Lower Plane |
NocoreStock | Returns or sets the Nocore Stock |
NumTabs | Returns or sets the Tab Points |
OptimizationMethod | Returns or sets the optim method |
Outtol | Returns or sets the outtol value |
RegionMethod | Returns or sets the Tab Points Region Method |
RetractPoint | Returns or sets the Retract Point |
RetractPointStatus | Returns or sets the Retract Point Status |
RetractPointToolAxis | Returns or sets the Retract Point Tool Axis |
RoughPasses | Returns or sets the Rough Passes |
SmoothLeadinDistance | Returns or sets the Smooth Leadin Distance |
SmoothLeadinFlag | Returns or sets the Smooth Leadin Flag |
SmoothLeadoutDistance | Returns or sets the Smooth Leadout Distance |
SmoothLeadoutFlag | Returns or sets the Smooth Leadout Flag |
StepoverBuilder | Returns the Stepover builder |
StopPointDistance | Returns or sets the Stop Point Distance |
StopPointFlag | Returns or sets the Stop Point Flag |
StopPointType | Returns or sets the Stop Point Type |
Tag | Returns the Tag for this object. |
ThreadHolePoint | Returns or sets the Thread Hole Point |
ThreadHolePointStatus | Returns or sets the Thread Hole Point Status |
ThreadHolePointToolAxis | Returns or sets the Thread Hole Point Tool Axis |
UpperPlane | Returns or sets the Upper Plane |
WireDiameter | Returns or sets the Wire Diameter |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
NocoreStock¶
-
WedmNocoreGeomBuilder.
NocoreStock
¶ Returns or sets the Nocore Stock
-------------------------------------
Getter Method
Signature
NocoreStock()
Returns: the Nocore Stock Return type: float New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
NocoreStock(nocoreStock)
Parameters: nocoreStock (float) – the Nocore Stock New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
Method Detail¶
Validate¶
-
WedmNocoreGeomBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.