TurnProbeInspectPointMoveBuilder Class¶
-
class
NXOpen.CAM.
TurnProbeInspectPointMoveBuilder
¶ Bases:
NXOpen.CAM.MoveBuilder
Represents the Turn Probe Inspect Point Move Builder
To create a new instance of this class, use
NXOpen.CAM.MoveCollection.CreateTurnProbeInspectPointMoveBuilder()
New in version NX8.5.1.
Properties¶
Property | Description |
---|---|
Direction | Returns or sets the probing direction |
FeedRate | Returns or sets the feed rate |
FeedType | Returns or sets the feed type |
FeedUnit | Returns or sets the feed unit |
MotionType | Returns or sets the motion type |
NumberOfUserParameters | Returns the number of user parameters |
Point | Returns or sets the point to probe |
ProbeControlParameters | Returns the probe control parameters builder |
ProbeProtectedParameters | Returns the probe protected parameters builder |
ProbeStockParameters | Returns the probe stock parameters builder |
ProbeToleranceParameters | Returns the probe tolerance parameters builder |
ProtectedMove | Returns or sets the protected move status |
SubopLabel | Returns or sets the subop label |
Tag | Returns the Tag for this object. |
Vector | Returns or sets the vector to define probing direction |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetUserParameter | Returns the custom parameter with the given name. |
ReverseDirection | Reversing the probing direction |
SetParent | Set parent |
SetSibling | Set sibling |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
TurnProbeInspectPointMoveBuilderDirectionTypes Enumeration | the probing direction type |
Property Detail¶
Direction¶
-
TurnProbeInspectPointMoveBuilder.
Direction
¶ Returns or sets the probing direction
-------------------------------------
Getter Method
Signature
Direction()
Returns: Return type: NXOpen.CAM.TurnProbeInspectPointMoveBuilderDirectionTypes
New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
Direction(dirType)
Parameters: dirType ( NXOpen.CAM.TurnProbeInspectPointMoveBuilderDirectionTypes
) –New in version NX8.5.1.
License requirements: cam_base (“CAM BASE”)
Point¶
-
TurnProbeInspectPointMoveBuilder.
Point
¶ Returns or sets the point to probe
-------------------------------------
Getter Method
Signature
Point()
Returns: Return type: NXOpen.Point
New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
Point(point)
Parameters: point ( NXOpen.Point
) –New in version NX8.5.1.
License requirements: cam_base (“CAM BASE”)
ProbeControlParameters¶
-
TurnProbeInspectPointMoveBuilder.
ProbeControlParameters
¶ Returns the probe control parameters builder
-------------------------------------
Getter Method
Signature
ProbeControlParameters()
Returns: Return type: NXOpen.CAM.ProbeControlParametersBuilder
New in version NX8.5.1.
License requirements: None.
ProbeProtectedParameters¶
-
TurnProbeInspectPointMoveBuilder.
ProbeProtectedParameters
¶ Returns the probe protected parameters builder
-------------------------------------
Getter Method
Signature
ProbeProtectedParameters()
Returns: Return type: NXOpen.CAM.ProbeProtectedParametersBuilder
New in version NX8.5.1.
License requirements: None.
ProbeStockParameters¶
-
TurnProbeInspectPointMoveBuilder.
ProbeStockParameters
¶ Returns the probe stock parameters builder
-------------------------------------
Getter Method
Signature
ProbeStockParameters()
Returns: Return type: NXOpen.CAM.ProbeStockParametersBuilder
New in version NX8.5.1.
License requirements: None.
ProbeToleranceParameters¶
-
TurnProbeInspectPointMoveBuilder.
ProbeToleranceParameters
¶ Returns the probe tolerance parameters builder
-------------------------------------
Getter Method
Signature
ProbeToleranceParameters()
Returns: Return type: NXOpen.CAM.ProbeToleranceParametersBuilder
New in version NX8.5.1.
License requirements: None.
Vector¶
-
TurnProbeInspectPointMoveBuilder.
Vector
¶ Returns or sets the vector to define probing direction
-------------------------------------
Getter Method
Signature
Vector()
Returns: Return type: NXOpen.NXObject
New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
Vector(vector)
Parameters: vector ( NXOpen.NXObject
) –New in version NX8.5.1.
License requirements: None.
Method Detail¶
ReverseDirection¶
-
TurnProbeInspectPointMoveBuilder.
ReverseDirection
¶ Reversing the probing direction
Signature
ReverseDirection()
New in version NX10.0.0.
License requirements: None.
Validate¶
-
TurnProbeInspectPointMoveBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.