ProbeProtectedParametersBuilder Class

class NXOpen.CAM.ProbeProtectedParametersBuilder

Bases: NXOpen.TaggedObject

Represents the Probe Protected Parameters Builder

New in version NX5.0.0.

Properties

Property Description
ApproachFlag Returns or sets the approach from clearance plane flag
ClearanceDistance Returns or sets the safe clearance distance for external features
CollisionFlag Returns or sets the collision flag
ReturnFlag Returns or sets the return to clearance plane flag
StandoffDistance Returns or sets the standoff distance
Tag Returns the Tag for this object.

Methods

Property Detail

ApproachFlag

ProbeProtectedParametersBuilder.ApproachFlag

Returns or sets the approach from clearance plane flag

-------------------------------------

Getter Method

Signature ApproachFlag()

Returns:
Return type:NXOpen.CAM.ProbeProtectedParametersBuilderAppMethodTypes

New in version NX5.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ApproachFlag(approachFrom)

Parameters:approachFrom (NXOpen.CAM.ProbeProtectedParametersBuilderAppMethodTypes) –

New in version NX5.0.0.

License requirements: cam_base (“CAM BASE”)

ClearanceDistance

ProbeProtectedParametersBuilder.ClearanceDistance

Returns or sets the safe clearance distance for external features

-------------------------------------

Getter Method

Signature ClearanceDistance()

Returns:
Return type:float

New in version NX5.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ClearanceDistance(clearanceDistance)

Parameters:clearanceDistance (float) –

New in version NX5.0.0.

License requirements: cam_base (“CAM BASE”)

CollisionFlag

ProbeProtectedParametersBuilder.CollisionFlag

Returns or sets the collision flag

-------------------------------------

Getter Method

Signature CollisionFlag()

Returns:
Return type:NXOpen.CAM.ProbeProtectedParametersBuilderCollisionFlagTypes

New in version NX5.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature CollisionFlag(collFlag)

Parameters:collFlag (NXOpen.CAM.ProbeProtectedParametersBuilderCollisionFlagTypes) –

New in version NX5.0.0.

License requirements: cam_base (“CAM BASE”)

ReturnFlag

ProbeProtectedParametersBuilder.ReturnFlag

Returns or sets the return to clearance plane flag

-------------------------------------

Getter Method

Signature ReturnFlag()

Returns:
Return type:NXOpen.CAM.ProbeProtectedParametersBuilderDepMethodTypes

New in version NX5.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ReturnFlag(returnTo)

Parameters:returnTo (NXOpen.CAM.ProbeProtectedParametersBuilderDepMethodTypes) –

New in version NX5.0.0.

License requirements: cam_base (“CAM BASE”)

StandoffDistance

ProbeProtectedParametersBuilder.StandoffDistance

Returns or sets the standoff distance

-------------------------------------

Getter Method

Signature StandoffDistance()

Returns:
Return type:float

New in version NX5.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature StandoffDistance(standoffDistance)

Parameters:standoffDistance (float) –

New in version NX5.0.0.

License requirements: cam_base (“CAM BASE”)