ProbeProtectedParametersBuilderCollisionFlagTypes Enumeration

NXOpen.CAM.ProbeProtectedParametersBuilder.CollisionFlagTypes is an alias for NXOpen.CAM.ProbeProtectedParametersBuilderCollisionFlagTypes

class NXOpen.CAM.ProbeProtectedParametersBuilderCollisionFlagTypes

Bases: object

the collision flag types

Enum Members

Enum Member Enum Member Description
Alarm
PATH OBSTRUCTED alarm
Flag
Error flag
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.