TurnAvoidanceDepartureBuilder Class

class NXOpen.CAM.TurnAvoidanceDepartureBuilder

Bases: NXOpen.TaggedObject

Represents an avoidance start of engage Builder

New in version NX6.0.0.

Properties

Property Description
DeparturePathMode Returns or sets the departure path mode
DeparturePathPointsListBuilder Returns the avoidance path points list builder
Tag Returns the Tag for this object.

Methods

Enumerations

TurnAvoidanceDepartureBuilderDeparturePathModes Enumeration The departure path mode options

Property Detail

DeparturePathMode

TurnAvoidanceDepartureBuilder.DeparturePathMode

Returns or sets the departure path mode

-------------------------------------

Getter Method

Signature DeparturePathMode()

Returns:the departure path mode value
Return type:NXOpen.CAM.TurnAvoidanceDepartureBuilderDeparturePathModes

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature DeparturePathMode(departurePathMode)

Parameters:departurePathMode (NXOpen.CAM.TurnAvoidanceDepartureBuilderDeparturePathModes) – the departure path mode value

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)

DeparturePathPointsListBuilder

TurnAvoidanceDepartureBuilder.DeparturePathPointsListBuilder

Returns the avoidance path points list builder

-------------------------------------

Getter Method

Signature DeparturePathPointsListBuilder()

Returns:the avoidance path points list builder
Return type:NXOpen.CAM.TurnAvoidancePathPointsBuilder

New in version NX6.0.0.

License requirements: None.