TurnAvoidanceDepartureBuilderDeparturePathModes Enumeration¶
NXOpen.CAM.TurnAvoidanceDepartureBuilder.DeparturePathModes is an alias for NXOpen.CAM.TurnAvoidanceDepartureBuilderDeparturePathModes
-
class
NXOpen.CAM.
TurnAvoidanceDepartureBuilderDeparturePathModes
¶ Bases:
object
The departure path mode options
New in version NX6.0.0.
Enum Members
Enum Member Enum Member Description NotSet Path is inactive.Points Path is defined by points.SameAsApproach Path is locked to approach path.PointsBeforeToolChange Path is defined by points, but applied only before tool change.SameAsApproachBeforeToolChange Path is locked to approach path, but applied only before tool change.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-