ToolAxisInterpolate Class¶
-
class
NXOpen.CAM.
ToolAxisInterpolate
¶ Bases:
NXOpen.TaggedObject
Represents a Tool Axis Interpolate Builder
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
InterpolationMethod | Returns or sets the interpolation method type |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
GetPoint | Get the point @return the point |
GetTotalNumberOfPoints | Get the total number of interpolate data points @return the total number |
ResetToDefault | The action of Reset to Default |
Enumerations¶
ToolAxisInterpolateInterpolateTypes Enumeration | the available types for Interpolate Types |
ToolAxisInterpolateInterpolationMethodTypes Enumeration | the available types for interpolate method |
Property Detail¶
InterpolationMethod¶
-
ToolAxisInterpolate.
InterpolationMethod
¶ Returns or sets the interpolation method type
-------------------------------------
Getter Method
Signature
InterpolationMethod()
Returns: the interpolation method type Return type: NXOpen.CAM.ToolAxisInterpolateInterpolationMethodTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InterpolationMethod(newValue)
Parameters: newValue ( NXOpen.CAM.ToolAxisInterpolateInterpolationMethodTypes
) – the interpolation method typeNew in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
Method Detail¶
GetPoint¶
-
ToolAxisInterpolate.
GetPoint
¶ Get the point
Signature
GetPoint(index)
Parameters: index (int) – the index of item Returns: the point Return type: NXOpen.Point
New in version NX7.5.5.
License requirements: None.