ToolAxisInterpolateInterpolationMethodTypes Enumeration

NXOpen.CAM.ToolAxisInterpolate.InterpolationMethodTypes is an alias for NXOpen.CAM.ToolAxisInterpolateInterpolationMethodTypes

class NXOpen.CAM.ToolAxisInterpolateInterpolationMethodTypes

Bases: object

the available types for interpolate method

Enum Members

Enum Member Enum Member Description
Linear
Linear
CubicSpline
Cubic Spline
Smooth
Smooth
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.