ThreadCutParameters Class¶
-
class
NXOpen.CAM.
ThreadCutParameters
¶ Bases:
NXOpen.CAM.CutParameters
Represents a
NXOpen.CAM.ThreadCutParameters
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
ChasePasses | Returns or sets the chase passes |
CheckIpwCollisions | Returns or sets the value to Check for Ipw Collsions |
CheckSafeClearance | Returns the Check Safe Clearance |
CutDepth | Returns the thread cut depth |
FinishPasses | Returns the finish passes |
HolderClearance | Returns the Holder Clearance |
IpwType | Returns or sets the IPW type |
NeckClearance | Returns the Neck Clearance |
NumberOfStarts | Returns or sets the number of starts |
PartSafeClearance | Returns the Part Safe Clearance |
PartStock | Returns the part stock |
PitchSetting | Returns the pitch setting |
ShankClearance | Returns the Shank Clearance |
Tag | Returns the Tag for this object. |
Tolerance | Returns the tolerance |
Tolerances | Returns the Tolerances builder |
UseToolHolder | Returns or sets the use tool holder |
Methods¶
Property Detail¶
ChasePasses¶
-
ThreadCutParameters.
ChasePasses
¶ Returns or sets the chase passes
-------------------------------------
Getter Method
Signature
ChasePasses()
Returns: the chase passes Return type: int New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ChasePasses(chasePasses)
Parameters: chasePasses (int) – the chase passes New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
CutDepth¶
-
ThreadCutParameters.
CutDepth
¶ Returns the thread cut depth
-------------------------------------
Getter Method
Signature
CutDepth()
Returns: the thread cut depth Return type: NXOpen.CAM.StepoverBuilder
New in version NX6.0.0.
License requirements: None.
FinishPasses¶
-
ThreadCutParameters.
FinishPasses
¶ Returns the finish passes
-------------------------------------
Getter Method
Signature
FinishPasses()
Returns: the finish passes Return type: NXOpen.CAM.TurnThreadFinishPassesBuilder
New in version NX6.0.0.
License requirements: None.
NumberOfStarts¶
-
ThreadCutParameters.
NumberOfStarts
¶ Returns or sets the number of starts
-------------------------------------
Getter Method
Signature
NumberOfStarts()
Returns: the number of starts Return type: int New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NumberOfStarts(startNum)
Parameters: startNum (int) – the number of starts New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
PitchSetting¶
-
ThreadCutParameters.
PitchSetting
¶ Returns the pitch setting
-------------------------------------
Getter Method
Signature
PitchSetting()
Returns: the pitch setting Return type: NXOpen.CAM.PitchSetting
New in version NX6.0.0.
License requirements: None.
Tolerance¶
-
ThreadCutParameters.
Tolerance
¶ Returns the tolerance
-------------------------------------
Getter Method
Signature
Tolerance()
Returns: the tolerance Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX6.0.0.
License requirements: None.