PitchSetting Class

class NXOpen.CAM.PitchSetting

Bases: NXOpen.TaggedObject

Represents a NXOpen.CAM.PitchSetting

New in version NX6.0.0.

Properties

Property Description
Distance Returns or sets the distance
End Returns or sets the end
Increment Returns or sets the increment
Option Returns or sets the pitch option
OutputUnit Returns or sets the output unit
Start Returns or sets the start
Tag Returns the Tag for this object.
ThreadPerUnit Returns or sets the thread per mm
Variance Returns or sets the pitch variance

Methods

Enumerations

PitchSettingOptionTypes Enumeration the pitch option types
PitchSettingOutputUnitTypes Enumeration the output unit types
PitchSettingVarianceTypes Enumeration the pitch variance types

Property Detail

Distance

PitchSetting.Distance

Returns or sets the distance

-------------------------------------

Getter Method

Signature Distance()

Returns:the distance
Return type:float

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Distance(distance)

Parameters:distance (float) – the distance

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)

End

PitchSetting.End

Returns or sets the end

-------------------------------------

Getter Method

Signature End()

Returns:the end
Return type:float

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature End(end)

Parameters:end (float) – the end

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)

Increment

PitchSetting.Increment

Returns or sets the increment

-------------------------------------

Getter Method

Signature Increment()

Returns:the increment
Return type:float

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Increment(increment)

Parameters:increment (float) – the increment

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)

Option

PitchSetting.Option

Returns or sets the pitch option

-------------------------------------

Getter Method

Signature Option()

Returns:the pitch option
Return type:NXOpen.CAM.PitchSettingOptionTypes

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Option(pitchOption)

Parameters:pitchOption (NXOpen.CAM.PitchSettingOptionTypes) – the pitch option

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)

OutputUnit

PitchSetting.OutputUnit

Returns or sets the output unit

-------------------------------------

Getter Method

Signature OutputUnit()

Returns:the output unit
Return type:NXOpen.CAM.PitchSettingOutputUnitTypes

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature OutputUnit(outputUnit)

Parameters:outputUnit (NXOpen.CAM.PitchSettingOutputUnitTypes) – the output unit

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)

Start

PitchSetting.Start

Returns or sets the start

-------------------------------------

Getter Method

Signature Start()

Returns:the start
Return type:float

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Start(start)

Parameters:start (float) – the start

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)

ThreadPerUnit

PitchSetting.ThreadPerUnit

Returns or sets the thread per mm

-------------------------------------

Getter Method

Signature ThreadPerUnit()

Returns:the thread per mm or inch
Return type:float

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ThreadPerUnit(thread)

Parameters:thread (float) – the thread per mm or inch

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)

Variance

PitchSetting.Variance

Returns or sets the pitch variance

-------------------------------------

Getter Method

Signature Variance()

Returns:the pitch variance
Return type:NXOpen.CAM.PitchSettingVarianceTypes

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Variance(pitchVariance)

Parameters:pitchVariance (NXOpen.CAM.PitchSettingVarianceTypes) – the pitch variance

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)