PitchSettingOptionTypes Enumeration

NXOpen.CAM.PitchSetting.OptionTypes is an alias for NXOpen.CAM.PitchSettingOptionTypes

class NXOpen.CAM.PitchSettingOptionTypes

Bases: object

the pitch option types

Enum Members

Enum Member Enum Member Description
Pitch
Pitch
Lead
Lead
ThreadsPerUnit
Threads per mm or inch
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.