SplitSubopCommand Class¶
-
class
NXOpen.CAM.
SplitSubopCommand
¶ Bases:
NXOpen.TaggedObject
Represents an Split Subop Command Builder
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
DividePlane | Returns or sets the divide plane |
EndPoint | Returns or sets the end point value |
LinePlaneType | Returns or sets the line plane type |
RotateAngle | Returns or sets the rotate angle value |
StartPoint | Returns or sets the start point value |
Tag | Returns the Tag for this object. |
Type | Returns or sets the split type |
Methods¶
Enumerations¶
SplitSubopCommandLinePlaneTypes Enumeration | Available line plane types |
SplitSubopCommandTypes Enumeration | Available split types |
Property Detail¶
DividePlane¶
-
SplitSubopCommand.
DividePlane
¶ Returns or sets the divide plane
-------------------------------------
Getter Method
Signature
DividePlane()
Returns: the divide plane Return type: NXOpen.Plane
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DividePlane(plane)
Parameters: plane ( NXOpen.Plane
) – the divide planeNew in version NX9.0.0.
License requirements: None.
EndPoint¶
-
SplitSubopCommand.
EndPoint
¶ Returns or sets the end point value
-------------------------------------
Getter Method
Signature
EndPoint()
Returns: the end point value Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndPoint(endPoint)
Parameters: endPoint ( NXOpen.Point
) – the end point valueNew in version NX9.0.0.
License requirements: None.
LinePlaneType¶
-
SplitSubopCommand.
LinePlaneType
¶ Returns or sets the line plane type
-------------------------------------
Getter Method
Signature
LinePlaneType()
Returns: the line plane type value Return type: NXOpen.CAM.SplitSubopCommandLinePlaneTypes
New in version NX9.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
LinePlaneType(type)
Parameters: type ( NXOpen.CAM.SplitSubopCommandLinePlaneTypes
) – the line plane type valueNew in version NX9.0.3.
License requirements: None.
RotateAngle¶
-
SplitSubopCommand.
RotateAngle
¶ Returns or sets the rotate angle value
-------------------------------------
Getter Method
Signature
RotateAngle()
Returns: the rotate angle value Return type: float New in version NX9.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
RotateAngle(rotateAngle)
Parameters: rotateAngle (float) – the rotate angle value New in version NX9.0.3.
License requirements: None.
StartPoint¶
-
SplitSubopCommand.
StartPoint
¶ Returns or sets the start point value
-------------------------------------
Getter Method
Signature
StartPoint()
Returns: the start point value Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StartPoint(startPoint)
Parameters: startPoint ( NXOpen.Point
) – the start point valueNew in version NX9.0.0.
License requirements: None.
Type¶
-
SplitSubopCommand.
Type
¶ Returns or sets the split type
-------------------------------------
Getter Method
Signature
Type()
Returns: the split type value Return type: NXOpen.CAM.SplitSubopCommandTypes
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(type)
Parameters: type ( NXOpen.CAM.SplitSubopCommandTypes
) – the split type valueNew in version NX9.0.0.
License requirements: None.